Engineering the future of HDD storage
Josh Roberts, Head of Applications Engineering at Festo says: “This was a tough project, with many automation challenges. It involved working across international borders, differing time zones, and language barriers — sometimes during the COVID-19 lockdown. Despite all these hurdles, we were able to push the automation envelope and deliver what we believe is the most advanced HDD automated storage and retrieval system in the world.”
‘Lights out’ ambition
The HDD manufacturer produces high-quality solid-state and hard disk drives for personal and enterprise use at its flagship facility in South East Asia. The factory makes around 400 million pieces per year. The production lifecycle of each piece is about 22 days, representing a significant quantity of work-in-progress at any one time. The objective was to reduce human interaction by automating the transfer of product between production cells before packing and shipping.
To improve safety and efficiency, the HDD manufacturer embarked on a three-year roadmap, aiming to create a fully automated ‘lights out’ factory environment. Automated Storage and Retrieval was central to delivering this vision. Dave Bowyer, head of DPB Automation, says: “Mechanical system development often involves developing an operating principle to go with it. Then follows the necessity for the drives and controls to operate the automation. Festo’s portfolio contained virtually everything we needed in this regard. Then, of course, we needed the right software to bring it to life.”
This is where Lumico, as the client’s incumbent software specialists, came into their own. Steve Kennington, co-founder and director of Lumico, recalls: “Integration with the existing factory automation software was crucial for success because this ‘parent’ system requests the material in and out of the ASRS. Our existing relationship with the client’s engineering teams was a big advantage because the trust was already there.”
Modular design
Delivering a ‘lights out’ operation for this customer demanded an ASRS with a capacity of 8,500 drives that could achieve rapid cycle times of 3.3–3.6 seconds from ‘product in’ to ‘product out.’ These speeds made it impractical to have one monolithic system. Instead, DPB Automation designed a modular system using a four-grid or six-grid configuration to optimise footprint and make use of the vertical space in the factory. There are six systems in all, each running on a cycle time of 19.8 seconds. A further requirement was a buffering capability to accommodate the difference between production rates and process cycle times.
Essentially, the ASRS comprises a large vertical array with a conveyor running through it. Each HDD on the conveyor is bar-coded, and the ASRS automatically identifies and picks product off the conveyor and loads it into the storage slots using pneumatics. Each piece is oriented and tilted to the correct angle, ready for the main handler to come and collect it for storage in the form of a grid. The cant of eight degrees ensures that the drives cannot work their way out of the disk drawers, providing an elegant alternative to using latches and closures on each slot, which would entail actuating each drawer. Gantry robots on the X and Z axes enable parallel operation of the modular units to achieve the desired capacity in the available space.
A further design consideration was that the new ASRS had to be static dissipative to prevent any electrical charge from damaging the HDDs. It therefore uses carbon-loaded plastic for the racking and grounded grid plates.
Automated speed and precision
The system incorporates Festo CMMT-AS multi-protocol servo motor controllers and Festo CMMT-ST multi-protocol 24 V DC servo controllers to achieve the necessary speed and precision when picking and placing the HDDs during storage and retrieval. However, this was no standard Cartesian handling system.
Dave Bowyer explains: “The conventional way to run a Cartesian handling system is to mechanically link the pair of actuators to a single motor so that they work as one. In this instance, it wasn't possible to do that because we couldn't have a mechanical tie across the base of the system. Also, it would have resulted in an extremely large motor that would have created power issues. So, we elected to have independent motors on each Z axis and run them in a master-slave control combination.”
In this configuration, the two Festo servo drives in each ASRS module are tied together with a communication link. The controller effectively interacts with one and the second one mimics it. Festo had to modify the software to enable its CMMT controllers to deliver the desired levels of performance.
Operational safety
Safe and efficient operation is an integral part of the final ASRS design. The master-slave configuration has a potentially high cost of failure because the machine would rip itself apart if the axes got out of phase. To minimise this risk, an ability to cope with a 200mm differential between the Z axes is built into the system. RH Electrical Engineering incorporated a laser beam sensing solution which monitors above and below the end effector for any offsetting and the ASRS will shut down immediately if the axes get out of sync. To avoid any crash risk, the beam detector also checks that no disks are protruding from the storage racks. LED lighting adds a final safety flourish. Running along each horizontal gantry beam, the LEDs give clear visual confirmation of the operational state of each ASRS module in the dark factory. A green light indicates the system is running as intended, blue indicates danger and red indicates a stoppage.
Successful outcome
The new ASRS took just nine months to deliver from a standing start – despite supply chain delays due to the pandemic. Following successful factory integration, the HDD manufacturer has been able to increase and improve manufacturing capacity. The barcoded products also improve traceability, which is crucial to gaining the environmental, sustainability, and quality certifications that are vital to securing future contracts.
About Festo
Festo is a global leader in automation technology setting international standards in industrial automation and technical education. The company provides pneumatic and electric automation solutions for factory and process automation across a wide range of industries.
Digitalisation, artificial intelligence and the rapidly growing LifeTech sector, including medical technology and laboratory automation, are becoming increasingly important areas of innovation for Festo. Sustainability, reducing its CO2 footprint, digital learning, innovation, performance and speed are key drivers for the company's future.
Festo products and services are available in 176 countries. With around 20,600 employees in more than 250 branch offices in around 60 countries, the company achieved a turnover of €3.33 billion in 2025. More than 8% of this is reinvested in research and development, and as a learning company, 1.5% of turnover is invested in basic and further training.
Festo Didactic, the company’s technical education and training division, is a leading global provider of technical training solutions, offering comprehensive digital and physical learning environments for industrial skills development.