2023/11/11
ID: 4614

Many functions safely under the roof of VTUX

Festo's new valve terminal VTUX combines the advantages of three classic valve terminals

Festo is now making it even easier for its users: the functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production.

The successor to the three valve terminal classics CPV, MPA-L/S and VTUG impresses with its high flow rate and almost limitless modularity. The valve terminal fits almost any machine concept. The valve terminal modules can be arranged as required. AP communication technology makes connections child's play, even over long distances. This communication technology creates the prerequisites for safety designs, predictive maintenance and data exchange with the cloud in the Industrial Internet of Things (IIOT).

 

Plug-in connections can be adapted to the desired hose diameter. This achieves an optimum balance between space saving and supply reliability. Any number of pressure zones can also be defined. The lightweight design of the VTUX allows it to be used on the front-end unit, a gantry or robot arm. This enables short and efficient pneumatic pipes.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The LifeTech sector with medical technology and laboratory automation is becoming increasingly important. The products and services are available in 176 countries. With about 20,800 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.81 billion in 2022. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
VTUX
VTUX: The new valve terminal combines the advantages of three classic valve terminals (photo: Festo)

Global Contact Person

Share Press Release