2020/05/12
ID: 2910

Quiet, fast, inexpensive: mass flow controller for life sciences

Proportional flow control valve VEMD with piezo technology

Whether in portable oxygen system devices or in bioreactors, the new proportional flow control valve VEMD from Festo provides extremely high control dynamics and costs considerably less than comparable solutions. Thank to piezo technology it requires only minimal space and power consumption.

The trend in life sciences is towards ever smaller medical devices, particularly for mobile applications such as portable oxygen system devices. The new mass flow controller VEMD from Festo enables even lighter, smaller and more energy-saving solutions to be designed. This increases the quality of life of patients who are dependent on such devices. The proportional flow control valve can support oxygen therapy devices during emergency ventilation and aftercare. Such applications are all the more important in the event of increased incidence of lung infections, such as during the current Covid 19 pandemic.

 

However, the proportional flow control valves are also ideal for use in bioreactors and fermenters for supplying cell cultures. They ensure a specific flow rate of process gases or create a protective atmosphere of nitrogen dioxide or carbon dioxide for industrial applications.

 

Piezo technology – compact, quiet, energy-efficient

The mass flow controller with piezo technology offers a wide variety of advantages, making it eminently suitable for life sciences and mobile applications. These include its silent operation, the absence of heat generation, the compact and lightweight design, the long service life and very low energy consumption. Especially the unmatched low power consumption of only one Watt opens up entirely new application options. Additionally, it is non-magnetic and doesn't interfere with any other medical equipment.

 

Easy to control, precise dynamics

The gas flow at the output of the valve can be adjusted very easily and controlled in linear mode by entering a setpoint between 0 and 10 V. An integrated control circuit with thermal sensor makes the VEMD precise and dynamic. It responds up to 35 times faster than comparable products to a setpoint change and is virtually immediately ready for operation.

 

Safe and reliable for all applications

High-tech piezo technology from Festo's LifeTech division can be adapted to meet the requirements of a very wide range of applications and customers. The expertise gained during intensive research and development in proportional control technology guarantees safe and reliable performance.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The LifeTech sector with medical technology and laboratory automation is becoming increasingly important. The products and services are available in 176 countries. With about 20,000 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €2.84 billion in 2020. Each year around 8 % of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
VEMD proportional flow control valve
Quiet, dynamic and cost-effective: the proportional flow control valve VEMD is a mass flow controller ideal for use in mobile devices.
© Festo SE & Co. KG
Portable oxygen system device
Increasing the quality of life in mobile applications with inaudible switching noises thanks to the quiet piezo technology.
© Festo SE & Co. KG
VEMD in ventilation treatment
Extremely high control dynamics: the proportional flow control valve VEMD is ideal for regulating gas flows in ventilation treatment.