Smart pipetting for safe laboratory processes
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and flexibility because of the changing fluid properties of the different media. Pressure-controlled liquid handling systems enable precise, scalable liquid handling. Festo has suitable solutions for these systems, whether for pipetting, dispensing or aspirating. Individual modules are available, such as the smart pipette head DHOP, but as well the complete multi-axis gantry EXCL, which can process several tasks at the same time thanks to two Z-axes.
Many life science applications rely on precise and repeatable liquid handling, whether for in vitro diagnostics or pharmaceuticals. Sample preparation processes often involve pipetting patient samples as well as dispensing and aspirating reagents in the microlitre range, all carried out in high throughput. Automated liquid handling robots overcome these challenges, but they are expensive and often include functions that are not needed. There is an alternative: pressure-controlled liquid handling systems. They offer a simple, fast and cost-effective way of precisely and reliably handling liquid volumes on a microlitre to millilitre scale by automating and linking sub-processes and, if needed, equipping them with the appropriate kinematics.
Intelligent pipetting
When pipetting sensitive patient samples and filling the microwell plates, it is important to avoid contamination and mixing DNA. The intelligent pipette head DHOP, set up with the finely tuned disposable tips DHAP from Festo, ensures reliable pipetting results. The plug and work solution is a closed-loop controlled pipette with proportional control with piezo technology. Many integrated functions optimise process reliability and simplify operation. This allows the smart pipette head to automatically set the specified target volume, independently of the liquid. Functions such as picking sensing and ejecting the disposable tips or the feedback about the pipetted volume have already been solved in the system.
Efficient dispensing and aspirating
In the next process step, reagents are added to the patient samples. Here, dispensing with a dispense head in the 9 mm grid of the microtitre plates is usually more efficient and reduces the process time. Different or identical liquids are distributed during this process step. This is where the pressure-controlled dispense head VTOE comes into its own: with up to eight channels, it offers many possible applications for precisely dispensing various liquids and filling quantities. The dispense head VTOI, on the other hand, distributes only one liquid. All eight outputs are controlled with just one valve. This means that larger flow rates are possible. Its design also allows it to be mounted in series, so that 12 valves can dispense 96 wells. When working with antigens or cultivating cells, liquids always need to be aspirated quickly and reliably. The dispense head VTOI is also suitable for this purpose, as it can be operated with vacuum.
Individually conceptualised and shipped ready-to-install
Reliability, precision and compact dimensions are key when handling liquids in laboratories. Instead of working with individual modules, users can also implement ready-to-install subsystems that have integrated, additional handling systems. Such a solution reduces the engineering effort and increases productivity, as all components are coordinated with each other. One example of this is the three-dimensional gantry EXCL with a small footprint and a motion/motor controller based on a highly integrated circuit board. The functionality of the system can be further extended with two independently traversable Z-axes. It is therefore ideal for analytical processes where sample vessels are to be opened and liquid samples pipetted in the same workspace.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.45 billion in 2024. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.