Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the cost and energy savings naturally result in lower CO2 emissions and higher productivity. Read press release Image Festo SE & Co. KG 2022/07/05 | Global How many users of compressed air know where the ... Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into ... Read press release
High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed energy efficiency to the top of the agenda in many companies. Festo Energy Saving Services to DIN EN ISO 11011 offer a customised range of services to provide support with this topic. As part of these services, energy efficiency experts from Festo work with customers and users to identify potential savings in how compressed air is used overall and reveal solutions to reduce consumption – now even with artificial intelligence. Read press release Image Festo SE & Co. KG 2022/07/05 | Global Identifying waste with artificial intelligence High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed ... Read press release
When it comes to reducing product-related CO₂ emissions, Festo can leverage two important aspects and also focuses on an all-encompassing approach to the CO₂ emissions caused by its products. The design of a machine lays the foundation of the CO₂ footprint at machine level. Festo supports this process first and foremost through free engineering tools. In addition, the key to a carbon-neutral future is to look at and assess CO₂ emissions from the point of view of the product, and then reduce these emissions with innovative solutions. Read press release Image Festo SE & Co. KG 2022/07/05 | Global Reducing CO₂ through sustainable engineering When it comes to reducing product-related CO₂ emissions, Festo can leverage two important aspects ... Read press release
Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is designed to meet the demanding specifications of modern production facilities. The new ELGT drive combines precision with high load-bearing capacity and rigidity, which makes it ideal for small parts and Lithium-ion battery manufacturing. Read press release Image Festo SE & Co. KG 2022/06/20 | Global Festo’s new ELGT cantilever electro-mechanical ... Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that ... Read press release
Handling the smallest amounts of liquids down to the microlitre range requires high levels of precision and flexibility because of the changing fluid properties of the different media. Pressure-controlled liquid handling systems enable precise, scalable liquid handling. Festo has suitable solutions for these systems, whether for pipetting, dispensing or aspirating. Individual modules are available, such as the smart pipette head DHOP, but as well the complete multi-axis gantry EXCL, which can process several tasks at the same time thanks to... Read press release Image Festo SE & Co. KG 2022/06/15 | Global Smart pipetting for safe laboratory processes Handling the smallest amounts of liquids down to the microlitre range requires high levels of ... Read press release
Festo is both a global player and an independent family-owned company based in Esslingen am Neckar, Germany. The company has become one of the global market leaders in its sector over the past 60 years thanks to its innovations and problem-solving competency, as well as a unique range of technical education. Festo has been developing components and system solutions for equipment manufacturers who specialise in the automation of laboratory processes and the manufacture of medical devices since 2004. Read press release Image Festo SE & Co. KG 2022/06/15 | Global The Festo Group Festo is both a global player and an independent family-owned company based in Esslingen am Neckar ... Read press release
The Festo Group has achieved the highest turnover in its history for the 2021 financial year. After a double-digit growth in turnover of around 18% to 3.36 billion euros (previous year 2.84 billion euros), the company started the first quarter with a double-digit order intake. This puts the innovation leader in automation and technical education in a good starting position to push ahead with its strategic orientation towards digitalisation and sustainability at full speed in 2022. The company expects further growth even under the current... Read press release Image Festo SE & Co. KG 2022/05/30 | Global Festo on course for growth The Festo Group has achieved the highest turnover in its history for the 2021 financial year. After ... Read press release
Finally, live on-site and hands-on: At Hannover Messe, visitors to Festo's Stand C22 in Hall 6 can once again experience the learning environments of Festo Didactic. Festo Didactic, the specialist for technical education and training, will be drawing highlights from its portfolio - from the Festo LX digital learning portal, the Festo Learning Experience, to learning systems and content focused on Electrical Engineering and Factory Automation. Read press release Image Festo Didactic SE 05/27/2022 | Global Competence development as an answer to the ... Finally, live on-site and hands-on: At Hannover Messe, visitors to Festo's Stand C22 in Hall 6 can ... Read press release
Algae are small climate savers. Even in their natural state they are extremely efficient photosynthesizers and absorb ten times more carbon dioxide (CO₂) than land plants. In bioreactors equipped with appropriate sensors, control technology and automation, the efficiency of algae can be increased to a hundred times that of land plants. This shows that they have a significant potential for a climate-neutral circular economy. With the PhotoBionicCell research project Festo demonstrates a potential approach for the industrial biologisation of... Read press release Image Festo SE & Co. KG 2022/05/27 | Global Automated cultivation of biomass Algae are small climate savers. Even in their natural state they are extremely efficient ... Read press release
Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the largest cork exporters worldwide. Although cork itself is light, it is all the more voluminous if it is packaged inefficiently. In order to save energy and CO₂ emissions during transport, the ESI Group developed a system for packaging corks that requires 30 per cent less packaging volume and does without plastic. On board: automation technology from Festo. Read press release Image Festo SE & Co. KG 2022/05/27 | Global Save 30 per cent volume Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are ... Read press release
The pneumatic extension modules VTOP from Festo enable custom closed-loop control solution designs in combination with a positioner, all without any external piping and the leaks associated with it. Compared with conventional solutions, cost savings of up to 30% are possible with the VTOP. And installation takes just a fraction of the time. Read press release Image Festo SE & Co. KG 2022/05/24 | Global Piping is now a thing of the past The pneumatic extension modules VTOP from Festo enable custom closed-loop control solution designs ... Read press release
The number of vehicles with electric powertrains is growing globally by more than 40% each year. At the same time, the manufacturing processes for the electrified powertrain are changing. While the classic manufacturing process for cars with internal combustion engines was predominantly based on semi-automatic production methods, both battery cells and electric motors are increasingly produced fully automatically. As a leading manufacturer of automation technology, Festo has the right solutions for this process along the entire value chain,... Read press release Image Festo SE & Co. KG 2022/05/23 | Global From battery cell production to the installation ... The number of vehicles with electric powertrains is growing globally by more than 40% each year. At ... Read press release
Festo and Q.ANT, a wholly owned subsidiary of TRUMPF, are entering into a strategic partnership to cultivate biomass on an industrial scale. The two companies aim to achieve this using a combination of automation technology from Festo and quantum technology from Q.ANT. Algae offers significant potential in this context. Read press release Image Festo SE & Co. KG 2022/05/23 | Global Q.ANT and Festo agree strategic partnership Festo and Q.ANT, a wholly owned subsidiary of TRUMPF, are entering into a strategic partnership to ... Read press release
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the cost and energy savings naturally result in lower CO2 emissions and higher productivity. Read press release Image Festo SE & Co. KG 2022/04/25 | Global How many users of compressed air know where the ... Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into ... Read press release
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging machines are on the safe side. This product combination from Festo guarantees compliance with food safety requirements. But Festo has suitable tubing/fitting combinations for other extreme situations too. Read press release Image Festo SE & Co. KG 2022/04/25 | Global On the safe side With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and ... Read press release
"For challenging tasks in thermoforming, ILLIG is your best bet," is a frequent refrain from manufacturers of branded goods. ILLIG Maschinenbau is a pioneer and market leader in the manufacture of machines and tools for producing plastic packaging using thermoforming. Its new thermoforming system RedLine RDF 85 now enables the use of off-system tool systems. This is how the company is setting new standards in flexibility. Also integrated is a stack handling system with electric axes from Festo. Read press release Image Festo SE & Co. KG 2022/04/25 | Global Compatible with many tools "For challenging tasks in thermoforming, ILLIG is your best bet," is a frequent refrain from ... Read press release