The preconfigured fail-safe circuit in the ready-to-install control cabinet is a safe and low-cost alternative when it comes to fail-safe technology. It replaces a single-acting actuator and guarantees that the actuator assumes a predefined safety position in the event of a pressure and/or power failure. Read press release Image Festo SE & Co. KG 2021/08/18 | Global Safety in fail-safe mode The preconfigured fail-safe circuit in the ready-to-install control cabinet is a safe and low-cost ... Read press release
The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up 75% less space than conventional plants, require just 50% of the energy and are also odour-free, while delivering excellent purification performance. Pneumatic automation technology from Festo ensures reliable and exact process sequences, while experts from Festo provide support with planning the plant. Read press release Image Festo SE & Co. KG 2020/09/22 | Global Nereda® technology for footprint and energy ... The patented Nereda process from Royal HaskoningDHV offers wastewater treatment plants that take up ... Read press release