2020/05/20
ID: 2951

Human-Robot Collaboration in Industry 4.0

In the ARIZ research project, Festo is working with partners to develop economical areas of application

The role of the human being in tomorrow’s production is often discussed. What new tasks will arise? Which of these can robots take on, and how will humans and robots work together? Festo is researching answers to these questions and other practical solutions together with partners from science and industry in the ARIZ project (“Work in the Industry of the Future”). In this context, the focus is on cost-effectiveness in addition to safety.

Machines and robots with extensive safety systems and suitable sensor technology enable humans and robots to move in the same work area and work together without safety barriers. In order to increase economic efficiency, the ARIZ project has set itself the goal of establishing a flexible and versatile production assistant in safe human-machine cooperation. This enables the demonstrator to be used at changing production workstations. It is intended to relieve the workload of employees by assisting and performing monotonous, ergonomically one-sided tasks.

 

A further project objective is to derive special qualification requirements for the employees who work with robots at these production workstations. Therefore, Festo Didactic is developing an appropriate learning system that optimally prepares employees for their tasks in the production of the future.

 

Robots as workers on the move

Until now, robots have usually only taken over one single programmed workflow. In this project, the partners are developing a demonstrator for highly versatile production: this robot should not be permanently installed in one location; rather, it should be mobile and flexible in use. It is connected to the higher-level IT system in order to be able to retrieve information and to simplify configuration for the operators.

 

Festo has successfully tested this application in the start-up stage – an area in which new technologies are tested before they are transferred to industrial production. In this area, an APAS robot from Bosch helps in the quality inspection of printed circuit boards. “We are currently further developing the concept of the ‘mobile robot worker’ in order to transfer the APAS robots to industrial production and electronic assembly. There, the robot will provide flexible support at various assembly workstations,” reports Michael Voß, ARIZ research engineer and project manager at Festo.

 

The challenge of increasing versatility

“The major challenges for assembly with robots are customized products with plenty of options in small batch sizes,” explains Michael Voß. “Only when the application is economical will automation make sense. For example, as few as possible different screw types and sizes should be used, so that the robot does not have to constantly change the screwdriver.”

 

With gripping tasks as well, standardisation is one key to success; however, there is also demand for universal solutions such as the DHEF – the adaptive shape gripper from Festo. This gripper uses the principle of the chameleon’s tongue to grip a wide variety of objects securely. With its elastic silicone cap, it can even pick up and deposit several objects in a single gripping process – without the need for manual modification.

 

Project partners

Together with Festo Automation, Festo Didactic is also involved in the ARIZ project. RWTH Aachen University is researching the effects of human-robot cooperation in terms of occupational science, for example concerning acceptance. robomotion GmbH develops assembly stations based on the concept of the mobile robot worker.

 

The consortium:

  • Festo AG & Co. KG
  • Festo Didactic SE
  • Human-Computer Interaction Center of the RWTH Aachen University (HCIC)
  • Institute for Enterprise Cybernetics e.V. of the RWTH Aachen University (IfU)
  • Chair of Information Management in Mechanical Engineering at RWTH Aachen University (IMA)
  • Center for Learning and Knowledge Management at RWTH Aachen University (ZLW)
  • robomotion GmbH
     
    The ARIZ project is funded under the number 01FG14003A by the BMBF (Federal Ministry of Education and Research) as part of the programme “Innovations for tomorrow’s production, services and work”.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.65 billion in 2023. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
Human-Robot Collaboration
The robot performs restacking tasks in the immediate vicinity of the worker, among other processes.
© Festo SE & Co. KG
Mobile robot worker
The robot as a mobile worker: it is not permanently installed but mobile and flexible for versatile production.
© Festo SE & Co. KG
Printed circuit boards
The APAS robot from Bosch supports quality inspection of printed circuit boards.

Global Contact Person

Share Press Release