Image
Festo AX Motion Insights Electric
Owner
Festo NAM
ID: 5114

Festo AI-Powered Electric Automation Monitoring Cuts Machine Downtime

Festo’s AX Platform delivers continuous monitoring of electric motion, transforming maintenance from reactive to predictive.

Festo introduces its AI-enables monitoring and predictive maintenance system Festo AX Motion Insights Electric. AX Motion Insights Electric is a cost-effective, easy-to-use solution for preventing costly unscheduled machine downtime through monitoring of electric axes and servo drives for wear and anomalies. This AI-based industrial app ensures operations are more reliable, efficient, and ultimately more profitable.

Motion Insights Electric enables maintenance teams to schedule tasks in advance, significantly reducing the risk of unexpected downtime. The platform offers the flexibility of on-premises computing, giving end users full control over their data and deployment. This is an open system and works with both Festo and third-party components. The AX platform features ease of use and seamless integration, opening the door for customers to embrace without worry today's AI, data-driven solutions, and digital transformation.

A critical element of Motion Insights Electric is its integration with Festo's Smartenance maintenance management system. Motion Insights Electric works in tandem with Smartenance; the insights app identifies when maintenance is needed, and Smartenance manages the resulting tasks. The integration of the two creates a cohesive, end-to-end workflow that ensures predictive insights are not just seen but also efficiently acted upon.

Motion Insights Electric is easy to set up and use. The "plug-an-play" aspect of this app, especially with Festo's CMMT multiprotocol servo drives, combined with its user-friendly interface and standardized AI models, makes the technology more accessible than otherwise possible. This is beneficial for original equipment manufacturers (OEMs) and end-use companies that are just beginning their digital journey, as it lowers the barrier to entry and brings the benefits of AI without requiring deep data-science expertise. OEMs and end users simply download the app, install it, and integrate it themselves. It's that easy,

Festo AX Motion Insights Electric joins the Festo AX Motion Insights Pneumatics app, which focuses on pneumatic component, and Festo AX Data Access, which makes operation technology (OT) data available for information technology (IT) analysis. Those apps can be used singly or in combination. CODI Manufacturing, Littleton, Colorado, recently installed all three on its new, compact gantry palletizer to give customers the ultimate in uptime and insights into operational efficiency.

The apps can be deployed on-premises using standard hardware and container technology like Docker. Containerization allows the apps to be deployed flexibility on various computing environments, including industrial PCs, virtual machines, servers, and edge devices. Insights Electric and Insights Pneumatic are purchased on a subscription basis while "time-limited" options (3 and 5 years) will be released at the end of 2025. Data Access is purchased under a perpetual license.

Through Festo App World, customers can select a license package based on the number of servo drives they want to monitor. Unlike competitors that might offer a single software tool, Festo AX apps are a seamless part of a complete one-stop-shop automation solution, including its electrical and pneumatic components. This simplifies integration and offers a single point of contact for support.

Contact a Festo sales representative or Festo distribution partner to learn more about Festo AX Motion Insights Electric and other AX apps. For more information on the advantages of working within the Festo ecosystem to leverage less engineering overhead, faster time to market, seamless connectivity, and high-quality components, visit www.festo.com.

AX Motion Insights Electric
AX Motion Insights Electric is a cost-effective, easy-to-use solution for preventing costly unscheduled machine downtime through its monitoring of electric axes and servo drives.