© Festo SE & Co. KG
VEFC mass flow controller
Compact and flexible thanks to piezo technology: the mass flow controller VEFC.
© Festo SE & Co. KG
2024/09/04
|
Irlande, Grande-Bretagne
Festo Controlled Pneumatics
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new ...
Lire le communiqué de presse
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new applications for pneumatics. The technology delivers more precision and control than ever, while having the potential to dramatically reduce energy use. This is clearly demonstrated in the VTEP: the first proportional valve terminal on the market, offering high precision, fast response times, and dynamic control.
French translation unavailable for Festo Introduces Pre-Configured and Assembled Air Preparation Units that Meet Safe Quality Food Guidelines.
© Festo SE & Co. KG
2024/06/06
|
Globale
Festo Expands its Portfolio with Multilayer Manifolds
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to ...
Lire le communiqué de presse
Festo is expanding its portfolio to include multilayer manifolds made of plastic (bonded manifolds) in order to be able to offer manufacturers of medical and laboratory equipment solutions from a single source. To this end, Festo is taking over the production systems and processes for manufacturing these complex plastic manifolds from Carville, a leading company in this field.
© Festo SE & Co. KG
Multilayer Manifold
Multilayer manifolds for manufacturers of medical and laboratory equipment: in future, Festo will offer these in combination with media-separated valves from a single source. 
© Festo SE & Co. KG
Battery Recycling
Recovering valuable lithium, cobalt, manganese and nickel from used batteries and reuse them for the production of new batteries: Automated recycling processes enable these rare minerals to be reused economically and cleanly. Festo has the right...
QM Systems 4
The high-speed vial filling, capping and labelling line designed by QM Systems.