Compact and leak-tight powerhouse
The media-separated solenoid valve VYKA from Festo allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates for so-called continuous flow applications. The excellent performance of this valve makes it suitable not only for laboratory applications, but also for the perfume and aroma industry as well as for packaging contact lenses.
For liquid and gas applications
The compact powerhouse VYKA doesn't only handle aggressive liquids, it is also perfect for gas applications thanks to its low leakage values. This is demonstrated by the helium test to which all valves are subjected after production. Customers with demanding requirements for the leak-tightness of valves, such as manufacturers of gas analysis equipment, can rely on VYKA.
Thanks to a separating diaphragm made of high-performance polymers EPDM, FKM and FFKM, the solenoid valve VYKA is also suitable for aggressive media. Since the designers have optimised the fluid space and the internal volume is low, the valve is easy to flush and clean. The combination with FDA-listed materials makes the VYKA ideal for highly sensitive applications. The current control ensures high reproducibility of the switching behaviour and leads to precise dosing and aspiration results. What's more, the holding current reduction of the plug-in electronics prevents sensitive media from heating up.
Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.33 billion in 2025. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.