New OVEH compact vacuum generator from Festo
The OVEH vacuum generator combines a compact design with advanced functionality, making it an ideal choice for a wide range of applications, including handling printed circuit boards, machine loading and unloading, packaging assembly, and picking finished items from 3D printers. Its universal robot interface, compliant with ISO 9409-1-50-4-M6, ensures compatibility with a variety of cobots and robots, enabling seamless integration into existing systems.
Peter Potters, Festo's EOAT Product Manager, explains: "The OVEH vacuum generator represents a significant step forward in EOAT technology. Its compact size, lightweight design, and integrated sensors make it a highly dynamic and reliable solution. Offering both high vacuum and high suction volume options, the OVEH provides manufacturers with the flexibility to adapt to diverse applications while maintaining process reliability."
The OVEH can be configured with a single suction cup or with up to nine suction cups on an adapter plate, offering a wide range of possible gripping positions. This flexibility allows manufacturers to create customised gripper units that can be easily retooled, adapting processes to meet demand. The OVEH’s low height and weight further contribute to its high dynamic response, making it well-suited for applications that require speed and precision.
Safe and reliable operation is assured with an integrated pressure sensor that continuously monitors vacuum levels. This feature is particularly valuable in applications where precision and consistency are critical. The OVEH vacuum generator also includes a valve-controlled ejector pulse, which enhances the secure handling of workpieces and supports efficient operation. Air quality is maintained using integral process air filters and an open silencer to reduce contamination of the suction nozzle.
Another standout feature of the OVEH is its plug-and-work capability. A mechanical robot interface enables quick and easy integration with various cobots, while control can be managed via digital I/O (PNP/NPN) or IO-Link®. Clearly designed interfaces simplify the connection of pneumatic tubing and a single electrical connector, reducing setup time and streamlining deployment.
Festo’s OVEH vacuum generator is a testament to the company’s commitment to developing EOAT solutions that empower manufacturers to optimise efficiency, enhance safety, and embrace the possibilities of human-robot collaboration. By combining cutting-edge technology with user-friendly design, the OVEH is poised to become a valuable asset in industries ranging from electronics and packaging to additive manufacturing.
For more information about the OVEH vacuum generator and Festo’s full range of EOAT solutions, visit: www.festo.com/eoat
Festo is a global leader in automation technology setting international standards in industrial automation and technical education. The company provides pneumatic and electric automation solutions for factory and process automation across a wide range of industries.
Digitalisation, artificial intelligence and the rapidly growing LifeTech sector, including medical technology and laboratory automation, are becoming increasingly important areas of innovation for Festo. Sustainability, reducing its CO2 footprint, digital learning, innovation, performance and speed are key drivers for the company's future.
Festo products and services are available in 176 countries. With around 20,600 employees in more than 250 branch offices in around 60 countries, the company achieved a turnover of €3.33 billion in 2025. More than 8% of this is reinvested in research and development, and as a learning company, 1.5% of turnover is invested in basic and further training.
Festo Didactic, the company’s technical education and training division, is a leading global provider of technical training solutions, offering comprehensive digital and physical learning environments for industrial skills development.