Solving simple motion tasks electrically is now possible with the Simplified Motion Series (SMS) from Festo. The electric drive series combines the simplicity of pneumatics with the benefits of electric automation to offer users an affordable solution that is easy to install and operate. The SMS consists of different linear and rotary electromechanical components together with a simple and application-optimised combination of motor and servo drives. With this solution, there is no need for external servo drives and the installation of a... Read press release Image Festo SE & Co. KG 2020/12/14 | South Africa Festo Simplified Motion Series electric drives ... Solving simple motion tasks electrically is now possible with the Simplified Motion Series (SMS) ... Read press release
Detecting irregularities at an early stage and initiating the necessary measures before a system failure are now made possible by the dashboards and IoT gateway CPX-IOT from Festo. The turnkey, preconfigured dashboards do not need any additional programming or installation of software. The collected data improves operating transparency for production managers and operators. Read press release Image Festo SE & Co. KG 2020/12/04 | South Africa Condition monitoring in the cloud Detecting irregularities at an early stage and initiating the necessary measures before a system ... Read press release
From manually operated to automated process valves, the new configurator tool for process valves from Festo makes selecting the right solution easy and less time-consuming. A task that used to take a few hours now takes minutes to complete. This configurator tool has made finding, selecting, sizing and ordering the perfect KVZB ball valve or KVZA butterfly valve simple with just a few clicks. All users have to do is select a few parameters, and the configurator will immediately suggest appropriate combinations, making engineering in the... Read press release Image Festo SE & Co. KG 2020/12/03 | South Africa Festo online configurator tool simplifies sizing ... From manually operated to automated process valves, the new configurator tool for process valves ... Read press release
The cloud is everywhere. We save data on the cloud and access it on our phones and computers from anywhere at our convenience. The same applies to seamless connectivity in industrial automation from your components to the cloud. This is why Festo considers your complete automation architecture from the mechanical system to the actuators, motors and servo drives, as well as the motion controllers, right up to modern industrial cloud solutions. Read press release Image Festo SE & Co. KG 2020/12/03 | South Africa Festo solutions make seamless integrated ... The cloud is everywhere. We save data on the cloud and access it on our phones and computers from ... Read press release
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells. Read press release Image Festo SE & Co. KG 06/01/2026 | Global Reliable degassing in battery cell production Degassing and sealing are core processes in battery cell production that directly follow the initial ... Read press release
Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Read press release Image Festo SE & Co. KG 05/29/2026 | Global Automated dismantling of electric batteries Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past ... Read press release
The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year until 2030. At the same time, the production processes for the electrified powertrain are changing. While semi-automated production processes have dominated traditional automotive manufacturing with combustion engines up to now, the manufacture of battery cells and electric motors is increasingly developing into fully automated production processes. As a leading manufacturer of automation technology, Festo has the right solutions for this along the... Read press release Image Festo SE & Co. KG 05/29/2026 | Global Everything under control from battery cells to ... The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year ... Read press release
Experts estimate that around 3 million tons of used batteries from electric cars will be due for recycling in 2030. This inevitably raises the question of sustainability, as batteries are energy storage devices made from critical raw materials. Festo therefore not only offers modular automation concepts for cell production, the assembly of battery modules and packs and for platform integration, but also for dismantling and recycling or separating the materials. Read press release Image Festo SE & Co. KG 05/29/2026 | Global Automated processes for battery recycling Experts estimate that around 3 million tons of used batteries from electric cars will be due for ... Read press release
05/29/2026 | Global The Battery Show Europe 2026 Visit Festo at the Stuttgart trade fair in hall 3 at stand E10 Press Releases (4) Images (16) View press kit Image Festo SE & Co. KG
04/24/2026 | Global Interpack 2026 7. until May 13, 2026, Messe Düsseldorf Press Releases (7) Images (16) View press kit Image Festo SE & Co. KG
04/17/2026 | Global Hannover Messe 2026 20. to 24. April 2026 – Welcome to Festo in Hall 13, Stand C17. Press Releases (6) Images (17) View press kit Image Festo SE & Co. KG
03/23/2026 | Global LogiMAT 2026 24. - March 26, 2026, Messe Stuttgart. You are cordially invited to visit the Festo stand: Hall 3, Stand 3D29. Press Releases (3) Images (5) View press kit Image Festo SE & Co. KG