Bild
Owner
Festo SE & Co. KG
ID: 3608

Hardware expertise paired with software and AI competence

AI software solutions for Predictive Maintenance, Predictive Quality and Predictive Energy
In its role as a technology and innovation leader in industrial automation and technical training, Festo aims to establish artificial intelligence (AI) as a key technology and core competence and to use it consistently for its customers' automation solutions. To this end, Festo offers intelligent solutions and services, with a focus on Predictive Maintenance, Predictive Quality and Predictive Energy.

Festo uses condition monitoring and machine learning in automation technology to monitor the behaviour of its customers' components, machines and systems. This means: making manufacturing processes more efficient and safer, improving quality, minimising production downtimes, waste and energy costs. “AI is the enabler that takes the automation business to a new level of efficiency. At Festo, we are able to provide end-to-end solutions for our customers thanks to the special constellation of hardware expertise in the field of electrical and pneumatic automation paired with software and AI expertise. Particularly in industrial intelligence, the mixture of algorithms paired with the specific expertise of an engineer is a decisive success factor for the implementation of AI-based automation applications. This is what sets Festo apart,” says Dr Frank Melzer, Member of the Management Board for Product and Technology Management. 

Three use cases in focus

Festo focuses on three use cases: Predictive Maintenance, Predictive Quality and Predictive Energy. The AI software solution “Festo AX”, which was developed by Festo and Resolto, a Festo subsidiary specialising in AI, is used here. “At its core, it is always the same challenge that we solve for our customers. We continuously monitor machine data and check it against our AI model, which describes the good state of a component or machine. The AI algorithms then detect deviations from the normal state and can also predict them,” says Dr Frank Melzer.

From simple condition monitoring of a machine or system to machine learning – depending on the application and the customer's goal, the software solution is adapted by Festo's application engineering experts and tailored to the customer's individual needs.

Example Automotive Industry

For example, a German automobile manufacturer uses Predictive Maintenance in car body construction. The customer's aim was to increase the efficiency of the maintenance of its servo-pneumatic welding guns by avoiding unforeseen downtimes as well as reducing service costs. Festo implemented algorithms to predict failures of the welding guns and integrated them into the existing infrastructure. Data from the welding guns is continuously collected and evaluated. After an evaluation of the data, failures could be identified before they actually occur. In this way, about a quarter of the downtimes in production could already be avoided, as the repair could be shifted to the non-production time.

Example Food & Packaging

Festo is currently using Predictive Energy for a customer in the Food & Packaging sector. The customer's goal: to reduce the energy consumption of its entire pneumatically operated bottling plant to a minimum in order to reduce CO2 emissions and save costs. First of all, Festo examined the entire compressed air process of the plant. The C2M energy efficiency module, which combines a pressure regulator, on-off valve, sensors and fieldbus communication in a single unit, monitors compressed air consumption, provides information about possible leaks and prevents the system pressure from falling below a defined standby pressure level. Thanks to the permanent condition monitoring of the system and the subsequent evaluation of the data via the AI software, the system reports deviations and faults in good time. In the future, the customer would also like to use the collected data for Predictive Maintenance.   

Open architecture of the AI solution

The architecture of Festo's AI solutions is scalable and can be flexibly deployed: On-Edge, On-Premise or in the Cloud. And it is an open architecture: Festo does not restrict its AI solutions to Festo components. Other components can also be easily integrated via IoT gateways and standardised protocols.

 

Press Photos and Captions

Title photo Welding Gun: 
Festo uses Predictive Maintenance in the automotive industry to increase efficiency in the maintenance of servo-pneumatic ​​​​welding guns by avoiding unforeseen downtimes and service and complaint costs. 
(Photo: Festo SE & Co. KG)

Dr Frank Melzer, Member of the Management Board for Product and Technology Management, Festo: 
“At Festo, we are able to provide end-to-end solutions for our customers thanks to the special constellation of hardware expertise in the field of electrical and pneumatic automation paired with software and AI expertise.” 
(Photo: Festo SE & Co. KG)

About Festo

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.33 billion in 2025. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

Title photo Welding Gun
Dr. Frank Melzer
Dr. Frank Melzer, Member of the Management Board Product and Technology Management, Festo SE und Co. KG