This content was translated automatically.

Image
Greifer Elektronik
Owner
Festo SE & Co. KG
ID: 5248

When robots grip intelligently, it’s all thanks to end-of-arm tooling

Intelligent gripping systems with software and AI make Festo a partner in robotics
A robot or handling system is only as good as the gripping system on its arm. End-of-arm tooling (EOAT) forms the interface with the workpiece and is what makes many automated processes possible in the first place. Festo offers more than just gripping components: The automation partner combines pneumatic and electric gripping solutions, as well as vacuum technologies, with robotics integration, software, and AI to create intelligent end-of-arm solutions.

From Grippers to Integrated End-of-Arm Solutions

Festo is evolving from a component supplier to a provider of integrated end-of-arm solutions and supports users from selection and design through integration to commissioning.

Standardized interfaces, engineering tools, and software modules simplify integration into robot systems from various manufacturers. This reduces the effort required for engineering, integration, and commissioning, allowing robotic applications to be implemented more quickly and easily.

Software and AI Make Gripping Smarter

Festo is consistently advancing the development of end-of-arm tooling through software and artificial intelligence. A robot should not only grip reliably, but also increasingly recognize on its own what needs to be gripped, where, and how.

One example of this is Vision Guided Motion (VGM). It combines intelligent image processing with precise path control. Components with varying positions and orientations are located and then processed using customer-configured programs (e.g., gluing or screwing) or gripped and transported to the next station. This reduces the need for mechanical adjustments and engineering effort while simultaneously increasing process reliability and productivity.
When dealing with unknown or varying objects, Festo takes it a step further with GripperAI: The AI-based software helps the robot recognize objects and determine suitable gripping points and strategies. This allows gripping processes to respond more flexibly to different objects. At the same time, the programming effort required for new applications is reduced.

It’s not just edible mushrooms that are within reach

The Mushroom Harvesting Unit demonstrates how AI and intelligent automation work together in practice. The solution combines image processing with motion and handling technologies for the automated harvesting of pressure-sensitive edible mushrooms. Using AI-powered image processing, the system detects and evaluates the mushrooms and determines the optimal harvest time. A high-precision gantry system positions the gripper over the target object. A rotating wrist axis and gentle gripping technology then enable damage-free harvesting.

End-of-arm tooling for a wide range of industries

Automated mushroom harvesting is just one example of the possibilities offered by modern end-of-arm technology. Gripping and vacuum solutions from Festo are used in numerous industries, such as the automotive industry, electronics manufacturing, packaging technology, the food industry, laboratory automation, and machine tools.

Whether delicate, heavy, small, irregularly shaped, or positioned in various ways—different workpieces require different gripping principles—all of which are implemented with end-of-arm solutions from Festo.

Festo at SPS: Hall 9, Booth 305

About Festo

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.33 billion in 2025. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

End-of-Arm Tooling in the Electronics Industry
High-precision and cost-efficient production of electronic components, whether for microelectronics, photovoltaics, or e-mobility. During the assembly and testing of electronic modules—including the assembly of irregular shapes—our systems ...
Mushroom Harvesting Unit with the HPSX Adaptive Gripper
The solution combines image processing with motion and handling technologies for the automated harvesting of pressure-sensitive edible mushrooms. Using AI-powered image processing, the system detects and evaluates the mushrooms and ...
Tool changers in machine tools
End-of-arm tooling enables the rapid, automated change of tools in machine tools.
End-of-arm tooling in the automotive industry
Suction spiders—specially developed vacuum-pneumatic grippers—move sheet metal components quickly and precisely in press shops and in body shop production. They ensure stable processes and enable fast cycle times. Ready-to-install systems ...