© Festo SE & Co. KG
Jürgen Lochner, CSO/CTO at ILLIG
"The development of sustainable packaging solutions is a priority for the experts in our ILLIG Technology Center," says Jürgen Lochner, Chief Sales Officer / Chief Technology Officer at ILLIG Maschinenbau GmbH & Co. KG.
© Festo SE & Co. KG
ILLIG stack handling system with Festo axes EGC-HD
Stack handling system: according to ILLIG, the electric axes EGC-HD with heavy-duty guide for high speeds and precision as well as the extremely rigid cantilever axis ELCC from Festo’s modular axis system proved to have the very high precision and...
© ILLIG Maschinenbau GmbH & Co. KG
ILLIG thermoforming system RDF 85
System with adaptive, variable tool interface: the flexibility of the new thermoforming machine RDF 85 from the RedLine product line enables tool systems from market competitors to be installed.
© ILLIG Maschinenbau GmbH & Co. KG
ILLIG thermoformed packaging
One thing ILLIG is particularly proud of is the ILLIG Technology Center: here, the company works with manufacturers of branded goods and packaging from the food and non-food area to test new packaging materials and shapes.
© Festo SE & Co. KG
2022/04/29
|
ワールドワイド
On the safe side
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging ...
プレスリリースを閲覧する
With the tubing PUN-H-F and the stainless-steel push-in fitting NPQR, manufacturers of food and packaging machines are on the safe side. This product combination from Festo guarantees compliance with food safety requirements. But Festo has suitable tubing/fitting combinations for other extreme situations too.
© Festo SE & Co. KG
Tubing PUN-H-F with push-in fitting NPQR
On the safe side: The combination of the tubing PUN-H-F and the stainless-steel push-in fitting NPQR from Festo guarantees compliance with food safety requirements for manufacturers of food and packaging machines.
© Festo SE & Co. KG
Tubing PUN-H-F
Tubing PUN-H-F: For highly versatile use in food applications, the “natural” colour variant can also be used in applications with gaseous oxygen.
© Festo SE & Co. KG
2022/04/11
|
ワールドワイド
Multifunctional in the smallest of spaces
The decentralised pressure and vacuum generator PGVA from Festo is a compact complete solution for laboratory ...
プレスリリースを閲覧する
The decentralised pressure and vacuum generator PGVA from Festo is a compact complete solution for laboratory automation. It integrates compressor, air preparation including filter system, reservoir and electronic pressure and vacuum control in the smallest of spaces.
© Festo SE & Co. KG
Screenshot GUI of pressure and vacuum generator PGVA
Simple: with a PC and the GUI software, the necessary parameters can be transferred via the COM or Ethernet port.