© Festo SE & Co. KG
Application Festo Motion Terminal VTEM pick & place
Highly flexible pick & place: the Festo Motion Terminal positions using pneumatics.
© Festo SE & Co. KG
VAEM valve controller
Small, light, energy efficient, fast, and precise ‒ the VAEM overcomes the challenges found in micro-dispensing liquids.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
2023/03/13
|
ワールドワイド
No longer afraid of the dentist
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants ...
プレスリリースを閲覧する
No one enjoys going to the dentist; young children even less so. To help future dentists and dental assistants deal with children during dental treatments, the Japanese company tmsuk has developed a humanoid robot that realistically simulates the behaviour of young children during these treatments, complete with fidgeting, flinching or closing the mouth. The dummy’s realistic movements are produced using proportional pressure regulators with ...
© Festo SE & Co. KG
VEAA/VEAB proportional pressure regulator
Silent, smooth and fast thanks to piezo technology: the VEAA/VEAB proportional pressure regulator.
Agitazione, movimenti improvvisi della bocca: il robot umanoide simula il possibile comportamento dei bambini durante un trattamento dentale.
© tmsuk, Japan
Pedia Roid Simulation of dental treatment 2
Fidgeting, twitching or sudden closing of the mouth: The humanoid robot for training purposes simulates the possible behaviour of children during a dental treatment.
© tmsuk, Japan
Pedia Roid Simulation of dental treatment 1
The Pedia Roid robot for training dentists and dental assistants: Piezo technology simulates lifelike movements.
Japanese translation unavailable for Festo Showcases its Latest Automation Innovations at Pack Expo Connects.
Japanese translation unavailable for Festo CPX-E/VTUG.
© Festo SE & Co. KG
2024/01/23
|
ワールドワイド
Reliable gripping without air
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. ...
プレスリリースを閲覧する
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required.