© Festo SE & Co. KG
Automotive Industry
The AI solution for clamping systems in the automotive industry prevents expensive machine failures.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
VUVG assembly line
Festo’s two-step production concept: In the first step, the Global Production Centers produce the basic product components efficiently and in high quantities. This production step is tailored to worldwide demand and does not tend to be linked to...
© Festo SE & Co. KG
Handling Guide Online Screen 1 DE
Handling Guide Online von Festo: Damit konfigurieren und bestellen Konstrukteure und Projekteure smart und intuitiv ihre neue Systemlösung – in gerade einmal 20 Minuten.
© Festo SE & Co. KG
Technology Plant VUVG assembly line control system
Festo products produce Festo products: on the left of the picture is a handling gantry, which could have been configured considerably faster using the Handling Guide Online.
© Festo SE & Co. KG
2020/07/30
|
ワールドワイド
The right handling system in just 20 minutes
As of immediately, technicians and engineers arrive at the right ready-to-install handling system at a ...
プレスリリースを閲覧する
As of immediately, technicians and engineers arrive at the right ready-to-install handling system at a record-breaking tempo in the areas of project engineering and planning. They can now order new system solutions intelligently and intuitively via the new Festo Handling Guide Online – without any interruptions in the value chain because the new configuration and ordering platform is integrated into the online product catalogue from Festo.
© Festo SE & Co. KG
Handling
With the Handling Guide Online, machine and equipment manufacturers are able to reduce time-to-market by the revolutionary amount of roughly 70% with regard to integrated handling systems.