Festo, der führende Anbieter für Automatisierungstechnik, erweitert sein Official Partner-Netzwerk und begrüßt Haberkorn Schweiz als neuen starken Partner. Diese Partnerschaft baut auf der bereits erfolgreichen Zusammenarbeit in Deutschland und Österreich auf und verstärkt die Präsenz von Festo in der Schweiz. Im heutigen Investitionsgütermarkt hat sich das hybride Kaufverhalten etabliert, bei dem Kunden Produkte aus verschiedenen Quellen beziehen. Dieser Trend wird von Festo bereits seit 2016 unterstützt, indem zusätzliche offizielle... Read press release Image Festo SE & Co. KG 2024/11/21 | Austria Germany Switzerland Festo erweitert Official Partner-Netzwerk in der ... Festo, der führende Anbieter für Automatisierungstechnik, erweitert sein Official Partner-Netzwerk ... Read press release
For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases. Read press release Image Festo SE & Co. KG 2023/11/09 | Global Germany A mass flow controller that is silent, fast and ... For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass ... Read press release
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. Read press release Image Festo SE & Co. KG 2023/11/08 | Global Germany A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... Read press release
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized pressure and vacuum generator PGVA from Festo. Read press release Image Sens 2023/11/08 | Global Germany Ensuring the right pressure Higher demands on throughput and precision – this is only possible with more automation in ... Read press release
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times and a long service life. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in the axis family ideal for use in cleanrooms. Read press release Image Festo SE & Co. KG 11/24/2025 | Global Precise and dynamic Innovative guide technology, high rigidity and guide load capacity for more load in the same ... Read press release
Festo is now making it even easier for its users: the proven advantages and all the useful functions of the classic valve terminals CPV, MPA-L/S and VTUG are now available under the umbrella of the convertible valve terminal VTUX. In addition, the AP-I and AP-A communication system creates the ideal platform for digitalized production. This provides flexibility, enables open architectures and the seamless integration of electrical and pneumatic automation. Read press release Image Festo SE & Co. KG 11/24/2025 | Global Many functions under one roof Festo is now making it even easier for its users: the proven advantages and all the useful functions ... Read press release
Long and complex engineering, programming and commissioning phases slow down many companies. With Festo AX Controls, Festo presents a real-time automation platform that addresses precisely this issue. It combines control, motion, AI, data integration and predictive maintenance in a flexible, scalable solution - perfectly tailored to the requirements of modern industry. Read press release Image Festo S.E. 11/24/2025 | Global Festo AX Controls brings fresh impetus to ... Long and complex engineering, programming and commissioning phases slow down many companies. With ... Read press release
Today, every machine must be analyzable in a standardized way - regardless of manufacturer or control system. Festo offers a broad portfolio of software and digital services for this purpose: from hardware-independent applications to device-related functions and apps through to digital twins. Read press release Image Festo SE & Co. KG 11/24/2025 | Global Rethinking digitalization Today, every machine must be analyzable in a standardized way - regardless of manufacturer or ... Read press release
11/23/2025 | Global SPS 2025 The automation trade fair in Nuremberg Press Releases (5) Images (9) View press kit Image Arturo Rivas
11/23/2025 | Global Productronica 2025 World's leading trade fair for the development and production of electronics Press Releases (5) Images (9) View press kit Image Sebastian Resch Photography
11/16/2025 | Global Compamed 2025 Compamed is the leading exhibition for high-tech solutions in the medical technology sector. Press Releases (4) Images (17) View press kit Image Messe Duesseldorf
2025/09/12 | Global Drinktec World’s Leading Trade Fair for the Beverage and Liquid Food Industry. Press Releases (4) Images (8) View press kit Image Festo SE & Co. KG