Naar verwachting zal het aantal voertuigen met elektrische aandrijving tot 2030 wereldwijd met ongeveer 30% per jaar toenemen. Tegelijkertijd veranderen de productieprocessen voor de geëlektrificeerde aandrijflijn. Terwijl semi-geautomatiseerde productieprocessen de traditionele autofabricage met verbrandingsmotoren tot nu toe domineerden, ontwikkelt de productie van batterijcellen en elektromotoren zich steeds meer tot volledig geautomatiseerde productieprocessen. Als toonaangevende fabrikant van automatiseringstechnologie heeft Festo... Persbericht lezen Afbeelding Festo SE & Co. KG 2026/05/29 | Global Alles onder controle, van batterijcellen tot ... Naar verwachting zal het aantal voertuigen met elektrische aandrijving tot 2030 wereldwijd met ... Persbericht lezen
Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for recycling in 2030. This inevitably raises the question of sustainability, as batteries are energy storage devices made from critical raw materials. Festo therefore not only offers modular automation concepts for cell production, the assembly of battery modules and packs and for platform integration, but also for dismantling and recycling or separating the materials. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/05/29 | Global Automated processes for battery recycling Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for ... Persbericht lezen
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Persbericht lezen
The success and reputation of electric vehicle manufacturers depend on the safe and flawless functioning of batteries. HAHN Automation Group has therefore developed a battery tester that carries out a complete test of the mobile energy storage units fully automatically. A 3-axis gantry for optical and leak tests, consisting of electric drives from Festo, takes centre stage. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/05/21 | Wereldwijd Safe batteries for electric vehicles The success and reputation of electric vehicle manufacturers depend on the safe and flawless ... Persbericht lezen
2024/11/07 | Global SPS 2024 - The Automation Summit in Nuremberg from ... The SPS from 12 – 14 November 2024 in Nuremberg is the industry highlight of the automation sector and, with its large ... Persberichten (7) Afbeeldingen (11) Persmap bekijken Afbeelding Festo SE & Co. KG
2024/05/28 | Global Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Persberichten (4) Afbeeldingen (15) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/05/22 | Global Battery Show Europe 2023 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Persberichten (5) Afbeeldingen (17) Persmap bekijken Afbeelding Festo SE & Co. KG
2023/03/17 | Global Tire Technology Expo 2023 March 21 to 23, 2023 Persberichten (3) Afbeeldingen (8) Persmap bekijken Afbeelding Festo SE & Co. KG