Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Persbericht lezen Afbeelding Festo SE & Co. KG 2024/02/15 | Wereldwijd Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Persbericht lezen
Opening sample vessels and pipetting liquid samples in the same workspace saves space in laboratories. This can now be achieved with the three-dimensional gantry EXCL from Festo, which has a small footprint for table-top devices and PCB-based motion control. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/11/08 | Wereldwijd Multiple functions in a small workspace Opening sample vessels and pipetting liquid samples in the same workspace saves space in ... Persbericht lezen
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo. Persbericht lezen Afbeelding Festo SE & Co. KG 2023/11/08 | Wereldwijd Duitsland A real modular DNA factory Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population ... Persbericht lezen
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files. Persbericht lezen Afbeelding Festo SE & Co. KG 2021/11/15 | Global The right handling system in a matter of minutes With the Handling Guide Online, design engineers can create the right ready-to-install handling ... Persbericht lezen
2025/06/23 | Wereldwijd Automatica exhibition 24-27 June 2025 in Munich/Germany Persberichten (6) Afbeeldingen (20) Persmap bekijken Afbeelding Festo SE & Co. KG
2025/02/10 | Wereldwijd LogiMAT March 11 - 13, 2025. Stuttgart Trade Fair Centre. You are cordially invited to visit the Festo Booth in hall 3, stand ... Persberichten (4) Afbeeldingen (10) Persmap bekijken Afbeelding Festo SE & Co. KG