The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Persbericht lezen Afbeelding Festo SE & Co. KG 2026/05/29 | Wereldwijd Automated dismantling of electric batteries The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past ... Persbericht lezen
A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo-pneumatic welding guns from Festo for many years. So much so that they have now installed more than 2,500 welding gun robots with this technology in the premium brand’s body shops. This car manufacturer has now been able to reduce downtimes by 25 percent thanks to a predictive maintenance system from Festo which is ready for artificial intelligence. Persbericht lezen Afbeelding Festo SE & Co. KG 2021/08/05 | Wereldwijd Servo-pneumatic welding guns from Festo reduce ... A leading car manufacturer has been relying on the pinpoint accuracy and efficiency of servo ... Persbericht lezen
2026/05/29 | Wereldwijd De batterijbeurs Europa 2026 Bezoek Festo op de beurs in Stuttgart in hal 3 op stand E10 Persberichten (4) Afbeeldingen (16) Persmap bekijken Afbeelding Festo SE & Co. KG