2020/03/04
ID: 2685

Reliably gripping and turning small parts

Compact rotary gripper module EHMD from Festo

The extremely compact rotary gripper module EHMD is the ideal choice in many applications where small objects need to be gripped and turned in confined spaces. For example, it can be used in laboratory automation to open small sample vials with ease. The Z module automatically adjusts to the thread pitches of the caps, eliminating the need for head/adapter changeover times.

Whether for in-vitro diagnostics, cell or genome research or quality inspections in the biotech and pharmaceutical industries, the rotary gripper module EHMD is completely reliable. This holds true for preparing and analysing samples, loading centrifuges, gripping, rotating and placing microwell plates or even opening and closing sample vials of different sizes.

Combined with a 3D gantry and a camera, it can support quality inspections with cameras, recognise bar codes, or print labels with a label printer. It is also perfect for use in light assembly or in the electronics industry.

Pneumatic or electric
The EHMD comes in two versions: fully electric or with a pneumatic gripper. Both permit infinite rotation. The optional assembly module with Z compensation automatically adjusts to the thread pitch of the caps without moving the Z-axis. When powered by the motor controller CMMO-ST from Festo, it allows sample containers of unknown size to be gripped with varying levels of force.

About Festo:

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The products and services are available in 176 countries. With about 21,000 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €3.07 billion in 2019. Each year around 8% of this turnover is invested in research and development. 

In this learning company, 1.5% of turnover is invested in basic and further training. Yet training services are not only provided for Festo’s own staff – Festo Didactic SE also supplies basic and further training programmes in the field of automation technology for customers, students and trainees.

© Festo SE & Co. KG
EHMD
The compact rotary gripper module EHMD comes in two versions: fully electric or with a pneumatic gripper.  
© Festo SE & Co. KG
EHMD in laboratory automation
The compact rotary gripper module EHMD from Festo can handle virtually any gripping task in laboratory automation, no matter how small.

Pessoa de contacto

Downloads

Partilhar comunicados de imprensa