© Festo SE & Co. KG Press Kit Hannover Messe 2022 Here you can find all Festo press releases for the Hannover Messe 2022 including our latest Bionic project, the first pneumatic robot and much more! Press Kit
© Festo SE & Co. KG 2022/07/18 | На глобальном уровне Sustainability at Festo - On the way to climate neutrality Automation is an enabler for the industrial transformation towards climate protection and resource efficiency, ... Читать пресс-релиз Automation is an enabler for the industrial transformation towards climate protection and resource efficiency, sustainability and the circular economy. With its products and solutions, Festo contributes to enabling resource-efficient production and helps to establish a circular economy along the entire value chain – with the clear aim of reducing CO2 emissions.
© Festo SE & Co. KG 2022/07/05 | На глобальном уровне Moving into the future with Controlled Pneumatics The production of tyres and the production of wafers seem to have absolutely nothing to do with each other. In ... Читать пресс-релиз The production of tyres and the production of wafers seem to have absolutely nothing to do with each other. In terms of automation technology, however, they use the same technology: Controlled Pneumatics. That is why Festo has further developed compressed air technology to make pneumatics sustainable, resource-saving and energy-efficient.
© Festo SE & Co. KG 2022/07/05 | На глобальном уровне How many users of compressed air know where the weak points in their systems ... Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the ... Читать пресс-релиз Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the ...
© Festo SE & Co. KG 2022/07/05 | На глобальном уровне Identifying waste with artificial intelligence High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed energy ... Читать пресс-релиз High energy prices, increasing cost pressure and the goal of climate-neutral production have pushed energy efficiency to the top of the agenda in many companies. Festo Energy Saving Services to DIN EN ISO 11011 offer a customised range of services to provide support with this topic. As part of these services, energy efficiency experts from Festo work with customers and users to identify potential savings in how compressed air is used ...
2022/07/05 | На глобальном уровне 19th International Press ... Sustainability in automation technology – more than a mega trend? Automation solutions may enable ... Пресс-релизы (8) Изображения (34) Видео (1) Просмотреть пресс-кит Просмотреть пресс-кит © Festo SE & Co. KG
2022/06/23 | На глобальном уровне Battery Show Europe 2022 28 to 30 June, 2022 Пресс-релизы (5) Изображения (20) Видео (0) Просмотреть пресс-кит Просмотреть пресс-кит © Festo SE & Co. KG
2022/06/16 | На глобальном уровне Analytica 2022 June 21st to 24th 2022 Пресс-релизы (6) Изображения (16) Видео (0) Просмотреть пресс-кит Просмотреть пресс-кит © Festo SE & Co. KG
2022/06/13 | На глобальном уровне Automatica 2022 June 21–24, 2022 | Trade Fair Center Messe München Пресс-релизы (5) Изображения (19) Видео (0) Просмотреть пресс-кит Просмотреть пресс-кит © Festo SE & Co. KG