2023/09/06
ID: 4118

A new era of human-robot collaboration: the first pneumatic cobot

The Festo Cobot sets new standards for technology and operability

What if there was a robot that was easy to operate, did not require a safety fence and was also attractively priced? That would introduce a whole new era in human-robot collaboration. This new era is dawning with the world's first pneumatic robot from Festo.

Hardly any industrial market segment will grow as rapidly over the next few years as human-robot collaboration. Cobots relieve employees of particularly strenuous or monotonous tasks, thus giving them new levels of freedom and making their work easier and healthier. And no other technology has such a sensitive and flexible approach to human-robot collaboration as pneumatics.

 

The benefits of pneumatics

The Festo Cobot owes many of its advantages, such as its sensitivity, weight and value for money, to the benefits of pneumatics. The direct drives in the articulated joints are very cost-effective and particularly lightweight because, unlike electric solutions, no heavy gear units or expensive force-torque sensors are required. The world's first pneumatic cobot is a result of the exceptional expertise in controlled pneumatics from Festo.

 

Cost-effective option – even for small and medium-sized companies

The Festo Cobot makes using cobots even cost-effective for small and medium-sized companies, as they often rely on manual work processes. This is achieved because of the flexible application options so that small batch sizes or work steps can also now be processed automatically. Thanks to its uniquely intuitive and simple commissioning and programming, it is quick and easy to get to grips with.

 

The pneumatic Festo Cobot will be cheaper than electric cobots in the same class. It will provide excellent value for money in its main application area of small parts handling with payloads of up to 3 kg. "The Festo Cobot will set new standards in human-robot collaboration with its ease of use," explains Gerhard Borho, Member of the Management Board Information Technology and Digitalisation.

 

Easy to operate and flexible to use

The Festo Cobot consists of the hardware itself, a handheld module and the Robotic Suite – software for intuitive commissioning and programming. This package makes it possible to commission and program the Cobot in less than an hour. Prior knowledge of robotics is not required either because the self-explanatory "Robotic Suite" software contains clearly visualised and standardised function blocks. Pneumatic drives enable the robot arm to be easily guided by hand and without any resistance so that waypoints or paths can be taught quickly and precisely.

 

Especially for small and medium-sized companies, cobots are only attractive if they can practically and quickly take on a new task and are not just intended to be permanently used for the same purpose. The Festo Cobot meets this requirement. Simple connections allow it to be used ad hoc without long changeover times. Common bus standards enable fast connection to higher-order controllers. 


Thanks to state-of-the-art, lightweight construction methods, the Festo Cobot weighs less than 20 kg – so that it can be used quickly and flexibly at another location.

 

Working safer and faster

With a length of 670 mm, the Festo Cobot is just like a human arm and has the right reach for it to be perceived as a helping third hand when working with a member of staff. It moves – like a real colleague – within a manageable radius. Thanks to the flexibility of the pneumatic drives, the cobot acts sensitively – at a speed appropriate to the situation and with fluid, harmonious movements. It is as soft to the touch as human contact.

 

The cobot's pneumatic direct drives and its light weight reduce its contact energy. Gerhard Borho, Member of the Management Board Information Technology and Digitalisation: "Thanks to precise pressure regulators in the articulated joints, the robot recognises when it is being touched and responds with appropriate safety functions." Employees can work together with their careful technical colleague in complete safety.

费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2022年,费斯托在全球61个国家的250多个分支机构拥有约20800名员工,实现销售额38.1亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。

© Festo SE & Co. KG
Festo Cobot_1
First pneumatic robot on the market: the Festo Cobot is easy to operate, does not require a safety fence and will be attractively priced.
© Festo SE & Co. KG
Festo Cobot_2
First pneumatic robot on the market: the Festo Cobot is easy to operate, does not require a safety fence and will be attractively priced.
© Festo SE & Co. KG
Gerhard Borho
Member of the Management Board Information Technology and Digitalisation, Festo SE & Co. KG