Reliable gripping without air
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. ...
阅读新闻稿
The electric standard gripper EHPS from Festo is the electric version of the pneumatic standard gripper DHPS. The EHPS can be used wherever pneumatics is not permissible. The concept of the electric standard gripper is based on simplicity and low complexity – all the electronics are integrated in the gripper, which means that an external motor controller is not required.