© Festo SE & Co. KG
Fast MDx - pipetting 2
The automated pipetting system, consisting of the pipetting head DHOE from Festo and the disposable syringe ejector DHAO, can accurately dispense volumes in the range of 10 µl.
© Festo SE & Co. KG
Fast MDx - pipetting 1
Space-saving: one gantry each takes care of pipetting and dispensing liquids as well as transporting and positioning the microwell plate.
© Festo SE & Co. KG
Fast MDx - testing system
High throughput: two 3D gantries with pipetting and transport units ensure a fully automated sequence of molecular diagnostic tests.
© Festo SE & Co. KG
2023/01/25
|
全球
Proportional valve technology makes it possible
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key ...
阅读新闻稿
The sustainability of cardboard packaging is leading to its increasing use instead of plastic packaging. A key step in the manufacture of folding boxes is the highly precise gluing of the box blanks. The company Baumer hhs is a specialist and global market leader for applications of this type with its dual-piston pump DPP – supported by the proportional valve VPPM from Festo.
© Festo SE & Co. KG
Baumer - gluing machine
Gluing machines achieve speeds of more than 700 metres per minute and can glue well in excess of 40,000 folding boxes per hour depending on the packaging size.
© Festo SE & Co. KG
Baumer - Marco Ahler
Marco Ahler, Technical Director at Baumer hhs
© Festo SE & Co. KG
Baumer - proportional pressure regulator VPPM
Proportional pressure regulator VPPM from Festo: the DPP piston pump regulates the air input pressure instead of the fluid pressure, and thus sets the required fluid pressure. The VPPM controls the air volume on the input side.
© Festo SE & Co. KG
Baumer - twin-piston pump DPP
Twin-piston pump DPP from Baumer hhs: the centrepiece of the gluing process – the proportional valve VPPM from Festo can be seen at the bottom of the photo.
© Festo SE & Co. KG
Baumer - high-precision gluing
High-precision gluing of folding boxes: systems from Baumer hhs make it possible to apply glue with millimetre accuracy without any contact with the blank, even at the highest production speeds.
Frugalpac 5
Festo’s CPX-E-CEC Controller regulates multiple axes simultaneously to achieve the complex curves on the glue paths, while Festo CMMT servo controllers are used for precise and repeatable loading, gluing and unloading.