© Festo SE & Co. KG
Process valve unit
Pre-assembled process valve units ensure that the components match one another properly, make installation easier and give you planning certainty, even in the case of customer-specific solutions.
© Festo SE & Co. KG
Nereda cycle
The Nereda technology is based on a simple cyclical process with three stages, which takes place in one or more Nereda reactors.
© Festo SE & Co. KG
Settling behaviour of Nereda granules
The sedimentation rate of the aerobic, granular biomass is up to thirty times faster in the Nereda process than in conventional plants.
© Festo SE & Co. KG
Nereda plant
The Nereda plant (centre bottom of picture, two large and one smaller round tank) needs more than 75% less space than the conventional plant (centre top of picture, surrounded by trees) while delivering the same purification performance.
© Festo SE & Co. KG
Automotive Industry
The AI solution for clamping systems in the automotive industry prevents expensive machine failures.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
VUVG assembly line
Festo’s two-step production concept: In the first step, the Global Production Centers produce the basic product components efficiently and in high quantities. This production step is tailored to worldwide demand and does not tend to be linked to...