Festo has introduced GripperAI, an AI-powered software solution that enables robots to handle mixed, unfamiliar and randomly positioned products without the need for extensive programming, template loading or specialist vision integration. Designed for manufacturers seeking greater flexibility from automated handling systems, GripperAI automatically identifies the optimum gripping point for each item and selects the most appropriate gripper for the task from the end-of-arm tools available. The software enables robots to adapt to changing... Read press release Image Festo SE & Co. KG 06/08/2026 | Ireland United Kingdom Festo launches GripperAI software Festo has introduced GripperAI, an AI-powered software solution that enables robots to handle mixed ... Read press release
Automation engineers are under increasing pressure to keep production running while managing ever more complex systems. Every minute of downtime counts, but critical technical information is often spread across multiple tools, manuals and data sources, slowing down troubleshooting and impacting productivity. Festo has introduced its new AI-powered Virtual Assistant to give engineers and maintenance teams immediate access to reliable technical answers, helping them resolve issues faster and keep operations moving. Read press release Image Festo SE & Co. KG 2026/04/30 | Ireland United Kingdom Festo launches an AI-powered Virtual Assistant Automation engineers are under increasing pressure to keep production running while managing ever ... Read press release
Festo has introduced the HPSX Universal Adaptive Gripper, a pneumatic soft gripper engineered to improve speed, hygiene and flexibility in demanding food, pharmaceutical and cosmetics applications. Combining robust design, food-safe materials and adaptive silicone fingers, the HPSX directly addresses long-standing automation challenges where rapid, precise and gentle product handling is essential. Read press release Image Festo SE & Co. KG 2026/03/24 | Ireland United Kingdom Festo Introduces the HPSX Universal Adaptive ... Festo has introduced the HPSX Universal Adaptive Gripper, a pneumatic soft gripper engineered to ... Read press release
Festo has expanded its VTUX valve terminal platform with a series of new functions and connectivity options that give machine builders greater design freedom, improved energy efficiency, and enhanced digital capability. Building on the highly cost-effective VTUX base system, the latest additions include advanced communication via Festo AP, new smart vacuum and I/O options, and new energy-saving valve functions. Together, these enhancements enable the creation of more compact, responsive and future-ready machines - reducing compressed air... Read press release Image Festo SE & Co. KG 2026/02/18 | Ireland United Kingdom Festo Expands VTUX Valve Terminal Festo has expanded its VTUX valve terminal platform with a series of new functions and connectivity ... Read press release
Two global players, one shared success story: In 2026, Festo will once again be Bosch’s Preferred Supplier for automation products in the “Pneumatic Components” category. This also makes Festo the first point of contact for new machine and plant projects. Bosch has relied on Festo for the eleventh consecutive year since 2015. Read press release Image Festo SE & Co. KG 07/17/2026 | Global Festo Once Again Named Bosch’s Preferred Supplier Two global players, one shared success story: In 2026, Festo will once again be Bosch’s Preferred ... Read press release
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells. Read press release Image Festo SE & Co. KG 06/01/2026 | Global Reliable degassing in battery cell production Degassing and sealing are core processes in battery cell production that directly follow the initial ... Read press release
Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Read press release Image Festo SE & Co. KG 05/29/2026 | Global Automated dismantling of electric batteries Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past ... Read press release
The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year until 2030. At the same time, the production processes for the electrified powertrain are changing. While semi-automated production processes have dominated traditional automotive manufacturing with combustion engines up to now, the manufacture of battery cells and electric motors is increasingly developing into fully automated production processes. As a leading manufacturer of automation technology, Festo has the right solutions for this along the... Read press release Image Festo SE & Co. KG 05/29/2026 | Global Everything under control from battery cells to ... The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year ... Read press release
05/29/2026 | Global The Battery Show Europe 2026 Visit Festo at the Stuttgart trade fair in hall 3 at stand E10 Press Releases (4) Images (16) View press kit Image Festo SE & Co. KG
04/24/2026 | Global Interpack 2026 7. until May 13, 2026, Messe Düsseldorf Press Releases (7) Images (16) View press kit Image Festo SE & Co. KG
04/17/2026 | Global Hannover Messe 2026 20. to 24. April 2026 – Welcome to Festo in Hall 13, Stand C17. Press Releases (6) Images (17) View press kit Image Festo SE & Co. KG
03/23/2026 | Global LogiMAT 2026 24. - March 26, 2026, Messe Stuttgart. You are cordially invited to visit the Festo stand: Hall 3, Stand 3D29. Press Releases (3) Images (5) View press kit Image Festo SE & Co. KG