脱气和密封是电池片生产中的核心工序,直接跟随着电池片与电压的初始接触。电池片被喷枪刺穿,接触过程中产生的成型气体被抽出。Festo 的气动和电动执行器用于处理和穿刺电池片。 阅读新闻稿 图像 Festo SE & Co. KG 2026/06/01 | 全球 电池生产中的可靠脱气 脱气和密封是电池片生产中的核心工序,直接跟随着电池片与电压的初始接触。电池片被喷枪刺穿,接触过程中产生的成型气体被抽出。Festo 的气动和电动执行器用于处理和穿刺电池片。 阅读新闻稿
Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that is designed to meet the demanding specifications of modern production facilities. The new ELGT drive combines precision with high load-bearing capacity and rigidity, which makes it ideal for small parts and Lithium-ion battery manufacturing. 阅读新闻稿 图像 Festo SE & Co. KG 2022/06/20 | 全球 Festo’s new ELGT cantilever electro-mechanical ... Industrial automation specialist Festo has introduced a new cantilever electro-mechanical drive that ... 阅读新闻稿
With the Handling Guide Online, design engineers can create the right ready-to-install handling system from Festo in record time, whether for a 2D linear and planar surface gantry, a 3D gantry or a new 3D cantilever system. Not only can they now plan extremely compact or extremely dynamic Cartesian robots using the intuitive configuration and ordering software, but they also benefit from the circuit diagram service from Eplan and commissioning files. 阅读新闻稿 图像 Festo SE & Co. KG 2021/11/15 | 全球 The right handling system in a matter of minutes With the Handling Guide Online, design engineers can create the right ready-to-install handling ... 阅读新闻稿
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a selection of the adhesive processes that represent the dosing and dispensing competencies of ViscoTec. Now the company has brought out cartridge applicator units designed for exact and clean feeding of adhesives, pastes and silicones of different viscosities, supported by a pneumatic control module supplied by Festo right to the ViscoTec assembly line as a ready-to-install module. 阅读新闻稿 图像 Festo SE & Co. KG 2021/11/09 | 全球 High-precision dosing with different viscosities Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are ... 阅读新闻稿
2023/11/13 | Global Productronica 2023 World's leading trade fair for electronics development and production where Festo shows latest innovations and solutions ... 新闻稿 (7) 图像 (22) 查看新闻稿资料 图像 Festo SE & Co. KG