Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
Přečíst tiskovou zprávu
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...