At SEMICON Europe 2026, Festo will demonstrate how wafers can be moved efficiently, precisely, and reliably through the semiconductor manufacturing process. A networked demonstration system illustrates the complete workflow—from the FOUP through wafer alignment to further processing in wet chemical or vacuum-based applications. Read press release Image Festo SE & Co. KG 11/06/2026 | Global End-to-End Wafer Handling Processes for Greater ... At SEMICON Europe 2026, Festo will demonstrate how wafers can be moved efficiently, precisely, and ... Read press release
The growing demand for specialized semiconductors—ranging from MEMS and SiC PowerChips to 2-nm GPUs and AI accelerators—is increasing the pressure on fabs and OEMs to operate their equipment cost-effectively while maintaining high process stability and repeatability. With solutions based on Controlled Pneumatics—a new generation of digitally controlled pneumatic technology—Festo helps machine builders and semiconductor manufacturers optimize process stability while reducing media consumption and energy usage. Read press release Image Festo SE & Co. KG 11/06/2026 | Global Digital Precision for Higher Wafer Yield The growing demand for specialized semiconductors—ranging from MEMS and SiC PowerChips to 2-nm GPUs ... Read press release
Festo aims to extend the quality standards applied to its hardware to digital product and simulation models. This will enable machine builders to develop and validate automation solutions virtually with the highest possible degree of realism. In the future, such models are also expected to support the development and testing of autonomous automation systems. Read press release Image Festo SE & Co. KG 10/21/2026 | Global Festo Develops Digital Twins for Physical AI Using ... Festo aims to extend the quality standards applied to its hardware to digital product and simulation ... Read press release
By combining the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel, Festo now offers a high-performance electric drive solution for the food, packaging, and pharmaceutical industries. Together with the appropriate motor cable, the motor, cable, and drive form a fully coordinated, complete hygienic design solution from a single source. Read press release Image Festo SE & Co. KG 10/19/2026 | Global Complete electric solution in hygienic design from ... By combining the EPRF electric cylinder and the EMMH servomotor, both made of stainless steel, Festo ... Read press release
11/06/2026 | Global Semicon Europe 2026 Semicon Europe is the largest European electronics platform, bringing together industry leaders from across the entire ... Press Releases (2) Images (4) View press kit Image Festo SE & Co. KG
05/29/2026 | Global The Battery Show Europe 2026 Visit Festo at the Stuttgart trade fair in hall 3 at stand E10 Press Releases (4) Images (16) View press kit Image Festo SE & Co. KG
04/24/2026 | Global Interpack 2026 7. until May 13, 2026, Messe Düsseldorf Press Releases (7) Images (16) View press kit Image Festo SE & Co. KG
04/17/2026 | Global Hannover Messe 2026 20. to 24. April 2026 – Welcome to Festo in Hall 13, Stand C17. Press Releases (6) Images (17) View press kit Image Festo SE & Co. KG