© Festo SE & Co. KG
Nereda plant
The Nereda plant (centre bottom of picture, two large and one smaller round tank) needs more than 75% less space than the conventional plant (centre top of picture, surrounded by trees) while delivering the same purification performance.
© Festo SE & Co. KG
Automotive Industry
The AI solution for clamping systems in the automotive industry prevents expensive machine failures.
© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
2020/08/03
|
Globálně
A global five stars system of production and logistics
The logistics and assembly plant in Mason close to Cincinnati/Ohio is the “North American brick” in ...
Přečíst tiskovou zprávu
The logistics and assembly plant in Mason close to Cincinnati/Ohio is the “North American brick” in Festo’s global production and logistics network. Now a majority of customers have available a Festo plant in a distance of a one-day-truck-drive. Let’s have a closer look to the Festo Value Production – “a five stars system of production and logistics”.
© Festo SE & Co. KG
Warehouse 2
Most modern logistics center outside of Germany: The Regional Service Center in Mason/Ohio which has many features that are usually only found in companies selling by catalogues, such as a top-mover area, automated order picking stations as well...
© Festo SE & Co. KG
Warehouse 1
Most modern logistics center outside of Germany: The Regional Service Center in Mason/Ohio which has many features that are usually only found in companies selling by catalogues, such as a top-mover area, automated order picking stations as well...