© Festo SE & Co. KG 2023/03/13 | Global Now with incident management and machine logbook With the maintenance software Smartenance, Festo has ushered machine and system maintenance into the digital ... Read press release With the maintenance software Smartenance, Festo has ushered machine and system maintenance into the digital era. Maintenance teams no longer need paper and pen, and long communication channels are a thing of the past. Festo now offers the software Smartenance with more functions and new licence packages.
© Festo SE & Co. KG 2020/05/20 | Global Cycle times reduced by 30 per cent Compact design for 30% shorter cycle times and 50% less vibration – those are the most important ... Read press release Compact design for 30% shorter cycle times and 50% less vibration – those are the most important characteristics of the cantilever axis with toothed belt ELCC-TB from Festo. The axis fits in seamlessly with Festo's concept of complete connectivity for its electric automation technology.
© Festo SE & Co. KG 2020/05/18 | Global The automated chameleon tongue Gripping workpieces just as a chameleon's tongue grips insects – that is the operating principle of ... Read press release Gripping workpieces just as a chameleon's tongue grips insects – that is the operating principle of the adaptive shape gripper DHEF from Festo. This unusual gripper can pick up, gather and set back down again objects of many different shapes without the need for manual adjustment.
© Festo SE & Co. KG 2020/04/09 | Global Chameleon’s tongue for industrial automation wins design prizes Grasping workpieces like a chameleon’s tongue – that’s the functional principle of ... Read press release Grasping workpieces like a chameleon’s tongue – that’s the functional principle of Festo’s adaptive shape gripper DHEF. The gripper can thus pick, gather and place objects of many different shapes without any need for manual changeovers. This is why it won renowned distinctions in 2020 including the iF Design Award and the Red Dot Design Award.
© Festo SE & Co. KG 2020/03/04 | Canada New Festo VMEF/VHEF manual or mechanically actuated valves deliver great ... Festo’s new VMEF/VHEF directional control valves put precision actuation literally at your fingertips, or ... Read press release Festo’s new VMEF/VHEF directional control valves put precision actuation literally at your fingertips, or even just a pinky.
© Festo SE & Co. KG 2020/02/12 | Canada Festo’s DLGF flat design rodless drive fits tight spaces and budgets Festo designed the new space-saving, flat, DLGF rodless linear drive Read press release Festo designed the new space-saving, flat, DLGF rodless linear drive
© Festo SE & Co. KG 2023/03/13 | Global SupraModule: Modulare Lösung für die Laborautomation In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the ... Read press release In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the cleaning of production facilities and their purity are very high. With superconductor technology, objects can be moved and handled without contact, which is ideal for such applications. At the Hannover Messe 2020 trade fair, Festo will be presenting the SupraModule concept, which enables wireless control of functions on a magnetic, floating carrier ...
© Festo SE & Co. KG 2020/01/08 | Canada Process Valve Configurator is Festo’s latest digital tool simplifying ... Festo Process Valve Configurator, process and application engineers can configure butterfly or ball valve ... Read press release Festo Process Valve Configurator, process and application engineers can configure butterfly or ball valve assemblies for their application online in just minutes.
© Festo SE & Co. KG 2020/11/26 | Global Ideal for automation in the chemical industry The quarter turn actuator DFPD-C from Festo is well equipped for the harsh conditions in the chemical industry. ... Read press release The quarter turn actuator DFPD-C from Festo is well equipped for the harsh conditions in the chemical industry. It is suitable for actuating butterfly valves, globe valves and ball valves in process plants in the chemical and petrochemical industry and can also be used with a positioner for control applications.