2020/02/12
ID: 2650

SupraModule: Modulare Lösung für die Laborautomation

New SupraMotion concept enables applications with wireless control

In future-oriented fields such as laboratory automation or biotechnology the requirements placed on the cleaning of production facilities and their purity are very high. With superconductor technology, objects can be moved and handled without contact, which is ideal for such applications. At the Hannover Messe 2020 trade fair, Festo will be presenting the SupraModule concept, which enables wireless control of functions on a magnetic, floating carrier with an autonomous energy supply.

Medical technology, laboratory automation, biotechnology and food production are decisive future fields of automation that have great growth potential for the coming decades. Contact-free, frictionless handling beyond walls and in any spatial orientation, which will become possible thanks to superconductor technology, will yield entirely new solutions – especially in highly pure environments. Reliable cleaning is essential for hygienically safe production in these applications.

Contact-free production of the future

The spatial separation of a product from its handling equipment in a vacuum, in a clean room, in gases or liquids ensures protected transport to meet the highest demands. The special characteristics of superconductors open great potential wherever contact-free bearing or handling is required. Automation can thus make inroads into areas of application that until now have been regarded as not or only hardly accessible to automation.

SupraModule – wireless control for variable functions

With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. The basis is a magnetic carrier with integrated control electronics and power supply. This floats at a distance of up to ten millimetres above a cryostat with superconductors. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper or a pipettor for laboratory applications. Thus, applications can be carried out in closed rooms with the SupraModule, which is particularly advantageous in laboratory automation and medical technology.

What are superconductors?

Superconductors are materials which below a certain temperature can store the field of a permanent magnet at a predefined distance. This effect enables objects to be held in position and manoeuvred without contact. The levitation gap remains stable even beyond walls. Thanks to their restoring forces, the superconductive magnetic bearing components autonomously return to their memorised position even after one of them is temporarily removed – entirely without external control engineering.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The LifeTech sector with medical technology and laboratory automation is becoming increasingly important. The products and services are available in 176 countries. With about 20,800 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.81 billion in 2022. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

SupraModule
© Festo SE & Co. KG
SupraModule 1
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_2
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_3
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.
SupraModule
© Festo SE & Co. KG
SupraModule_4
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.