With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable packaging material, low energy consumption, high speed and ergonomics, the CABLIblue 870 card-to-card blister system is proving to be a real trendsetter. The use of electrical automation technology from Festo increases sustainability and efficiency immensely in this application. Read press release Image Festo SE & Co. KG 04/24/2026 | Global How packaging machines are becoming more ... With the blister packaging machine from IWK, sustainability is not just lip service: with recyclable ... Read press release
Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries. Read press release Image Festo SE & Co. KG 2024/02/15 | Global Moving loads at the tip of two fingers Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in ... Read press release
Standardisation is a recipe for success for a fruitful collaboration between packaging machine manufacturers and automation specialists. The strategic partnership between Syntegon and Festo is a great example of this. Thanks to this cooperation, Syntegon was able to simplify its processes and manage the challenges posed by the pandemic and the supply chain crisis more effectively. Read press release Image Festo SE & Co. KG 2023/05/03 | Global Standardisation benefits all packaging lines Standardisation is a recipe for success for a fruitful collaboration between packaging machine ... Read press release
04/24/2026 | Global Interpack 2026 7. until May 13, 2026, Messe Düsseldorf Press Releases (7) Images (16) View press kit Image Festo SE & Co. KG
2023/05/04 | Global Interpack 2023 International trade fair for the global processing and packaging industry Press Releases (6) Images (24) View press kit Image Festo SE & Co. KG