© Festo SE & Co. KG
BionicFinWave
The fins of the BionicFinWave are cast out of silicone and do not require struts or support elements.
© Festo SE & Co. KG
BionicFinWave
The underwater robot BionicFinWave manoeuvres itself independently through a pipe system made of acrylic glass.
© Festo SE & Co. KG
VEAE in ventilator breathing devices
The proportional valve VEAE is suitable for portable or stationary ventilator breathing devices for outpatient or hospital use.
© Festo SE & Co. KG
VEAE proportional valve
The proportional valve VEAE from Festo reliably and precisely regulates gas flows, whether oxygen, air, nitrogen or inert gases.
Supra Drive 2.0
© Festo SE & Co. KG
SupraDrive 2.0
With superconductor technology, objects can be stored and moved without contact – as with the SupraDrive 2.0.
SupraMultitool
© Festo SE & Co. KG
SupraMultitool
At the SupraMultitool exhibit, a handling system positions a workpiece carrier on two different magnets in turn.
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_2
Sensors and camera systems register the positions of the operator, components and tools at the BionicWorkplace.
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_3 Sprachsteuerung
Humans can intuitively control the BionicCobot in the BionicWorkplace by means of gestures, touch or speech.
BionicWorkplace
© Festo SE & Co. KG
BionicWorkplace_1
BionicWorkplace: A human works together with a bionic robotic arm, along with numerous assistance systems and peripheral devices that are conntected and communicate with each other.
SupraModule
© Festo SE & Co. KG
SupraModule_4
With the SupraModule, different applications can be carried out with the same system in a floating position and controlled wirelessly. Depending on requirements, different systems can be attached to the carrier, for example a compact gripper.