Thanks to radio-based indoor GPS with ultra-wideband technology (UWB) the BionicSwifts can fly safely and in a coordinated pattern in a defined airspace. To execute these flight manoeuvres as true to life as possible, the wings are modelled on the plumage of real birds. The agility of the artificial birds is not just due to their lightweight design and aerodynamic kinematics, but also to the use of function integration. Leer nota de prensa Imagen Festo SE & Co. KG 2020/07/01 | Global Artificial feathers give flight to robotic birds Thanks to radio-based indoor GPS with ultra-wideband technology (UWB) the BionicSwifts can fly ... Leer nota de prensa
Industrial change demands a new kind of interaction between people, machines and data. In the future, operators and robots will work ever more closely together. This is why Festo has been working intensively on systems which, for example, can relieve people of monotonous or hazardous activities while at the same time posing no risk. Artificial intelligence plays a central role here. The BionicMobileAssistant is a prototype of a robot system that moves independently in three dimensions and can identify objects, grip adaptively and work together... Leer nota de prensa Imagen Festo SE & Co. KG 2020/07/01 | Global Mobile robot system meets BionicSoftHand 2.0 Industrial change demands a new kind of interaction between people, machines and data. In the future ... Leer nota de prensa
Agarrar piezas como la lengua de un camaleón: el principio activo de la pinza de forma adaptativa DHEF de Festo imita el funcionamiento de la lengua de un camaleón. Esto le permite agarrar, recopilar y depositar objetos con formas diferentes sin necesidad de una conversión manual. Por ello ha recibido los galardones de renombre mundial iF Design Award y Red Dot Design Award en el año 2020. Leer nota de prensa Imagen Festo SE & Co. KG 2020/04/09 | Global La lengua de camaleón de la automatización gana ... Agarrar piezas como la lengua de un camaleón: el principio activo de la pinza de forma adaptativa ... Leer nota de prensa
Short product life cycles and a high diversity of variants are requirements brought about by industrial change. At the same time, it is becoming increasingly important to ensure that employees can rapidly and intuitively adapt to new tasks. This calls for new forms of collaboration between people, machinery and software. A key role is played here by self-learning systems with artificial intelligence and by robot-based automation solutions that can work hand in hand with the human operator and can form networks with each other. All these... Leer nota de prensa Imagen Artist 2018/04/23 | Global BionicWorkplace: Human-robot collaboration with ... Short product life cycles and a high diversity of variants are requirements brought about by ... Leer nota de prensa