Image
Owner
Festo SE & Co. KG
ID: 3093

New Festo VMEF/VHEF manual or mechanically actuated valves deliver great precision

Mississauga, ON, March 2020 – Festo’s new VMEF/VHEF directional control valves put precision actuation literally at your fingertips, or even just a pinky. A single finger can be used to activate these valves – or a hand, or a workpiece making contact with a trigger mechanism. 

These valves are based on touch actuation with minimal force – there is no energy to convert, no long cables or additional response time. They perform functions that directly result in a followup action, like clamping or closing safety doors (if manually actuated) or acting as a signal generator (if mechanically actuated). The actuated stem switches the valve and triggers that next step in the process.

For manual actuation, the VHEF offers a choice of “triggers” ¬– a finger, handle or toggle lever or a pushbutton. VMEF offers a stem, roller-lever or one-way roller-level actuation. 

These ergonomic manual/mechanical valve series have a robust metal housing and are capable of withstanding sudden, significant force to allow for occasional rough treatment. They can be installed without backlash in just a few simple steps. And they are attractively priced.

All configurations are available as 3/2 way and 5/2 way valves with G1/8 and G1/4 connections as well as NPT variants. More variants like 5/3 way valves are available, depending on model selected.
 

Keywords
Personne de contact
Natasha
Gosine