Image
Owner
Festo SE & Co. KG
ID: 4686
Hannover Messe Press Preview 2024
February 21st 2024 in Hannover, Germany
The future of our planet also presents Festo with major challenges. On the one hand, it is about supplying the world's population and coping with demographic change, and on the other hand, it is about protecting our natural resources and CO2-neutral production. With our "Blue World" approach, we want to express how we can balance these challenges with the help of automation technology and technical education.
Communiqués de presse
Télécharger tout le contenu (env. 58.93 Mo)
Keywords
Personne de contact
Elke
Schwarzenberger