The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Lire le communiqué de presse Image Festo SE & Co. KG 2026/05/29 | Global Automated dismantling of electric batteries The manual dismantling of end-of-life batteries in electric vehicles is now a thing of the past ... Lire le communiqué de presse
On prévoit une croissance annuelle d'environ 30% du nombre de véhicules à propulsion électrique dans le monde d'ici 2030. Parallèlement, les processus de production pour la chaîne cinématique électrifiée se transforment. Alors que les procédés de production semi-automatiques dominaient jusqu'à présent dans la construction automobile classique avec des moteurs à combustion, la fabrication de cellules de batteries et de moteurs électriques évolue de plus en plus vers des processus de production entièrement automatisés. En tant que fabricant... Lire le communiqué de presse Image Festo SE & Co. KG 29.05.2026 | Globale Tout sous contrôle, des cellules de batterie aux ... On prévoit une croissance annuelle d'environ 30% du nombre de véhicules à propulsion électrique dans ... Lire le communiqué de presse
Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for recycling in 2030. This inevitably raises the question of sustainability, as batteries are energy storage devices made from critical raw materials. Festo therefore not only offers modular automation concepts for cell production, the assembly of battery modules and packs and for platform integration, but also for dismantling and recycling or separating the materials. Lire le communiqué de presse Image Festo SE & Co. KG 2026/05/29 | Global Automated processes for battery recycling Experts estimate that around 3 million tonnes of used batteries from electric cars will be due for ... Lire le communiqué de presse
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce compressed air consumption by up to 50%. Lire le communiqué de presse Image Festo SE & Co. KG 2024/02/05 | Globale Pneumatics Makes a Technological Leap with Piezo Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up ... Lire le communiqué de presse
29.05.2026 | Globale The Battery Show Europe 2026 Visitez Festo au salon de Stuttgart, hall 3, stand E10 Communiqués de presse (4) Images (16) Voir le dossier de presse Image Festo SE & Co. KG
2025/06/23 | Global Automatica exhibition 24-27 June 2025 in Munich/Germany Communiqués de presse (6) Images (20) Voir le dossier de presse Image Festo SE & Co. KG
2024/05/28 | Global Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Communiqués de presse (4) Images (15) Voir le dossier de presse Image Festo SE & Co. KG
22.05.2023 | Global Battery Show Europe 2023 Fiable, économique, durable : Le cycle de vie circulaire des batteries - des solutions de la production des cellules ... Communiqués de presse (5) Images (17) Voir le dossier de presse Image Festo SE & Co. KG