© Festo SE & Co. KG
2022/01/31
|
Irlande, Grande-Bretagne
Design Cartesian robots in minutes
Festo has extended the capabilities of its Handling Guide Online (HGO) to include 3D cantilever systems in ...
Lire le communiqué de presse
Festo has extended the capabilities of its Handling Guide Online (HGO) to include 3D cantilever systems in addition to linear, planar surface and 3D handling systems. These improvements mean that design engineers can now plan extremely compact or extremely dynamic Cartesian robots in a matter of minutes using the HGO’s intuitive configuration and ordering software. They can also benefit from the complete documentation package, including circuit ...
Handling Guide Online 2
Dynamic cartesian configurations in the Handling Guide Online. Top row: 2D linear and gantry robots. Bottom row: 3D gantry and cantilever systems.
© Festo SE & Co. KG
Handling Guide Online 1
Extremely compact or extremely dynamic Cartesian robots can now be configured in a matter of minutes using Festo’s Handling Guide Online.
© Festo SE & Co. KG
Cobot E30
Magswitch E-Series intelligent magnetic grippers reduce end-effector size, lower cycle time, ensure safety, and offer new solutions. Shown here is the CoBot SmartMagGrip E30 for collaborative robotic applications.Magswitch E-Series intelligent...
© Festo SE & Co. KG
2021/11/15
|
Globale
Le meilleur système de manipulation en quelques minutes
Avec HGO, les concepteurs peuvent créer en un temps record le bon système de manipulation Festo, ...
Lire le communiqué de presse
Avec HGO, les concepteurs peuvent créer en un temps record le bon système de manipulation Festo, prêt à installer, qu'il s'agisse d'un portique linéaire 2D, d'un portique 3D ou d'un nouveau système en porte-à-faux 3D. Non seulement ils peuvent désormais concevoir des robots cartésiens extrêmement compacts ou extrêmement dynamiques à l'aide de ce ...
© Festo SE & Co. KG
“Handling Guide Online”, le Guide de la manipulation en ligne
Grâce au Handling Guide Online, les constructeurs de machines et de systèmes sont en mesure de réduire jusqu'à 70 % le délai de mise sur le marché des systèmes de manipulation intégrés.
2021/10/20
|
Irlande, Grande-Bretagne
Grolsch bottling plant upgrade goes with a swing, thanks to Festo automation
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ...
Lire le communiqué de presse
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager. The ‘swing-top transfer unit’ was custom-designed by Festo in conjunction with system integrator MCA Linear Motion Robotics and is installed at the Grolsch Enschede plant in The Netherlands.
© Festo SE & Co. KG
Grolsch pic 2
The Grolsch 'swing-top transfer unit' features the new Festo EMMT servo motor and CPX-E automation system and provides approximately 3,800 bottles per hour with a porcelain cap and rubber ring.
Grolsch pic 1
New servo technology from Festo is helping Grolsch to put the iconic swing tops on its bottles of lager.