VEMD: proportional control valve
The new VEMD proportional flow control valve from Festo offers extremely high control dynamics combined with minimal space and power consumption requirements.  
BionicSwift pic 2
Les ailes modelées sur le plumage de vrais oiseaux améliorent l'efficacité et les performances de vol.
BionicSwift pic 1
La mise en réseau intelligente et la navigation GPS 3D pourraient être utilisées dans les usines en réseau du futur.
2020/06/17
|
Irlande, Grande-Bretagne
Mini factories in containers help reduce face mask shortages
Protective masks have been in short supply in these times of coronavirus. An innovative containerised ...
Lire le communiqué de presse
Protective masks have been in short supply in these times of coronavirus. An innovative containerised production facility that enables businesses and healthcare organisations to produce their own masks to order could solve the problem. Developed in just six weeks by Mikron with engineering support from Festo, the mini factory uses a scalable system that can produce 50-100 face masks per minute.
© Festo SE & Co. KG
BionicSwift pic 3
BionicSwift Festo - une étude robotique dans des structures aérodynamiques légères.
Face mask - CMMT-ST pic 3
Compatible with higher-level controllers from Beckhoff, Siemens or Rockwell: the CMMT servo drive from Festo.
Face mask_DFM pic 2
Products from Festo’s core range, like the DFM guided drive shown here, enabled the face mask manufacturing system to be built quickly and reliably.
Face mask production system pic 1
Fits in a 20-foot shipping container: Mikron’s system for producing 50-100 protective masks a minute.