Bild
Owner
Festo SE & Co. KG
ID: 4602

A mass flow controller that is silent, fast and cost-effective

Proportional flow control valve VEMD from Festo precisely controls air and gases
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.

In many industrial applications, the flow of air or other gases must be regulated. In food production, biotechnology or the chemical industry, the control of oxygen, air, CO2 and inert gases is an integral part of daily production. As a rule, the gases must be dosed precisely and with a high degree of repeat accuracy. The high demands on reliability and robustness are just as important as cost efficiency. The new VEMD offers both: high dynamics at an affordable price.

 

As part of the biologization of our economy, biotechnological production processes are increasingly coming into focus. The VEMD proportional flow control valves are ideal for use in bioreactors and fermenters. They supply the microorganisms and cell cultures with the required gases. The devices are also suitable for applications where initial inertization of a container is necessary or where a protective atmosphere of nitrogen or carbon dioxide is required as part of production processes. Typical processes in a protective atmosphere include filling processes in the pharmaceutical, chemical and food industries. It is also used in additive manufacturing, commonly referred to as 3D printing.

 

Proportional control

The gas flow at the output of the mass flow controller can be easily adjusted and linearly controlled using a setpoint specification. Various analog (0-10V, 1-5V, 4..20mA) and digital interfaces such as Ethernet/ModBus TCP and RS232/RS485 with ModBus RTU are available for this purpose. Further advantages of the VEMD mass flow controller are fast control, noiseless operation, compact and lightweight design, long service life and low energy consumption.

 

Dynamic and precise

Thanks to the integrated control circuit with thermal sensor, the VEMD works precisely and dynamically. It reacts quickly to setpoint changes. The VEMD is available in flow ranges of 100 l/min and 200 l/min. The current flow rate value is transmitted to the higher-level control system as an output value. It can optionally be read off the display on site at any time. Further variants with 50 l/min. as well as 10 l/min. and 20 l/min. will be available on the market in the course of 2024.

 

About Festo

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,600 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.33 billion in 2025. More than 8% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

VEMD proportional flow control valve
The proportional flow control valve VEMD is a mass flow controller that is silent, dynamic and affordable, and thus ideal for use in the life sciences, food production or biotechnology.