© Festo SE & Co. KG
2023/11/08
|
ワールドワイド, ドイツ語
A mass flow controller that is silent, fast and cost-effective
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow ...
プレスリリースを閲覧する
 For the gas supply of bioreactors and fermenters or for dosing protective gases - the VEMD mass flow controller from Festo delivers maximum control dynamics and costs significantly less than comparable solutions for the control of air, oxygen and inert gases.
© Festo SE & Co. KG
2024/05/06
|
ワールドワイド, ドイツ語
A real modular DNA factory
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate ...
プレスリリースを閲覧する
Seeds are the new gold. Why is that? Plant-based foods can feed an ever-growing world population. But climate change, pests and diseases threaten plant breeding. To help develop resistant seeds and make them available to agriculture, plant breeders need vast amounts of DNA. That is precisely why Synchron Lab has developed the "DNA factory", which is automated with handling gantries, electric axes, pneumatic grippers and sensors from Festo.
© Sens
2023/11/08
|
ワールドワイド, ドイツ語
Ensuring the right pressure
Higher demands on throughput and precision – this is only possible with more automation in laboratory ...
プレスリリースを閲覧する
Higher demands on throughput and precision – this is only possible with more automation in laboratory technology. Sensapex already equips more than 800 customers worldwide with high-precision micromanipulators, microscopes, and pressure controllers – from neuroscience research to in vitro fertilization (IVF) – to name only a few application examples. To work successfully the pressure controllers from Sensapex rely on the decentralized ...
Japanese translation unavailable for Mit neuen Ideen für mehr Wettbewerbsfähigkeit.
Japanese translation unavailable for Festo und Winkelmann bei der Vertragsunterzeichnung.