© Festo SE & Co. KG
FinRay Gripper
The FinRay gripper from Festo offers gripper fingers that adapt to the workpiece. This allows safe and tactile gripping of workpieces with plastic malleability such as pouch cells.
© Festo SE & Co. KG
CPX-AP-I
The remote IO system CPX-AP-I seamlessly integrates all IOs and IO-Link participants such as sensors and valve terminals into the communication network of the plant. This ensures seamless communication from the workpiece to the cloud.
© Festo SE & Co. KG
Cantilever handling system spindle axes ELGT
A cantilever handling system based on spindle axes ELGT ensures dynamic and safe loading and unloading of the process chamber.
© Festo SE & Co. KG
Degassing process chambers
The core of the application is the process chamber. Pneumatic and electric actuators manipulate hollow lances and pierce the battery cells.
© Festo SE & Co. KG
2023/05/15
|
ワールドワイド
Reliable degassing in battery cell production
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting ...
プレスリリースを閲覧する
Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells.
© Festo SE & Co. KG
Martin Stadler, ViscoTec
Martin Stadler, Managing Director of ViscoTec
© Festo SE & Co. KG
Christian Heidinger, ViscoTec
Christian Heidinger, Head of Product Management at ViscoTec
© Festo SE & Co. KG
2021/11/09
|
ワールドワイド
High-precision dosing with different viscosities
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a ...
プレスリリースを閲覧する
Precisely gluing smartphone displays, applying thermal paste or gluing micro cameras in place are just a selection of the adhesive processes that represent the dosing and dispensing competencies of ViscoTec. Now the company has brought out cartridge applicator units designed for exact and clean feeding of adhesives, pastes and silicones of different viscosities, supported by a pneumatic control module supplied by Festo right to the ViscoTec assembly ...
© Festo SE & Co. KG
Control module for ViscoTec
The heart of the system: the control module supplied ready for installation by Festo monitors the pressure and quality of the adhesive application independently of temperature and viscosity.
© Festo SE & Co. KG
Dashboard Festo and FlexFactory
Festo's maintenance software Smartenance collects data and makes it available to FlexFactory's Risk Balance Board via a Digital Financial Twin. This allows individual process steps on the shop floor to be evaluated and continuously...