© Festo SE & Co. KG
Bionics4Education_1
Bionics4Education: An integral didactic concept comprising learning kits and a digital learning environment.
© Festo SE & Co. KG
2023/01/13
|
ワールドワイド
Unique forms of motion derived from nature
Walking and rolling like the flic-flac spider – the BionicWheelBot moves along the ground in astounding ...
プレスリリースを閲覧する
Walking and rolling like the flic-flac spider – the BionicWheelBot moves along the ground in astounding ways. Together with the team headed by the discoverer of the spider, Professor Ingo Rechenberg, Festo has taken a very close look at these unique forms of locomotion and has technically realised them. But no magnifying glass was needed for the flying fox: the BionicFlyingFox is an imposing figure with its wingspan of 2.28 metres and its partly ...
© Festo SE & Co. KG
BionicFlyingFox 2
The wing kinematics of the BionicFlyingFox are also divided into primaries and secondaries.
© Festo SE & Co. KG
BionicFlyingFox 1
Despite its wingspan of 228 cm and its overall length of 87 cm, the BionicFlyingFox weighs 580 grams.
© Festo SE & Co. KG
BionicWheelBot 2
The BionicWheelBot in rolling mode with extended propelling legs.
© Festo SE & Co. KG
BionicWheelBot 1
Mechatronic overall system: intricate kinematics based on a natural model.
© Festo SE & Co. KG
University SLP 4
Qualification of students in the Festo Authorized and Certified Training Centre (FACT) at the Universidad Politecnica de San Luis Potosí.
© Festo SE & Co. KG
Dual Year
Qualification 4.0 for Mexico: Working via German Chamber of Commerce (AHK), German Society for International Cooperation (GIZ) and Federal Institute for Vocational Education and Training (BIBB), Germany is among the countries supporting the...
© Festo SE & Co. KG
Mechatronics for kids
Technical education for Mexico: Festo’s “Automation and Mechatronics for kids” events, in which over 1,000 children and young people from all over Mexico take part every year, are a great success. Picture: Event 2016 in Mexico City as part of the...
© Festo SE & Co. KG
Festo Ballooning
Festo Ballooning at the foot of one of the largest buildings of antiquity, the pyramid of Teotihuacán in Mexico.