© Festo SE & Co. KG
Recirculating conveyor system
Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button.
© Festo SE & Co. KG
Multi-Carrier-System® 3
Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button.
© Festo SE & Co. KG
Gripper system
High flexibility: Different box sizes and the matching number of products are set directly in the Multi-Carrier-System® MCS using the freely positionable carriers. The products can be individually transported, grouped and synchronously packaged on...
© Festo SE & Co. KG
VTEM and MCS complete system
Format change at the push of a button: two Festo innovations enable fast and straightforward format changes on just one machine – the Festo Motion Terminal VTEM and the Multi-Carrier-System® MCS.
© Festo SE & Co. KG
DGST compact slide - 2
Introducing the industry’s most compact slide unit – the DGST, along with a new range of compact cylinders and guided cylinders to provide the ideal drive combination for compact assembly systems.
© Festo SE & Co. KG
ELCC cantilever axis
ELCC cantilever axis from Festo can cut cycle times in handling applications by up to 30%.
DFPC pneumatic linear actuator
Freedom of choice: The double-acting pneumatic linear actuator DFPC from Festo for process valves is available either as low-cost, preconfigured standard variants from stock or as individually configured versions.
© Festo SE & Co. KG
2020/04/09
|
ワールドワイド
Chameleon’s tongue for industrial automation wins design prizes
Grasping workpieces like a chameleon’s tongue – that’s the functional principle of ...
プレスリリースを閲覧する
Grasping workpieces like a chameleon’s tongue – that’s the functional principle of Festo’s adaptive shape gripper DHEF. The gripper can thus pick, gather and place objects of many different shapes without any need for manual changeovers. This is why it won renowned distinctions in 2020 including the iF Design Award and the Red Dot Design Award.
© Festo SE & Co. KG
DHEF Adaptive Shape Gripper 1
Adaptive shape gripper DHEF: like a chameleon’s tongue, it reliably grasps irregular, round and sensitive objects. Festo’s gripper won the internationally acclaimed iF Design Award and Red Dot Design Award for this extraordinary gripping concept.
© Festo SE & Co. KG
Cabinet Guide Online 2
Numerous custom control cabinet variations possible with the online tool Cabinet Guide Online. (Image: Festo SE & Co. KG)