ELGD Toothed Belt
© Festo SE & Co. KG
2024/11/08
|
ワールドワイド
Precise and dynamic
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space ...
プレスリリースを閲覧する
Innovative guide technology, high rigidity and guide load capacity for more load in the same installation space - these are the features of the new ELGD axis family from Festo. In addition, powerful drive elements offer high feed forces and accelerations for shorter cycle times, a long service life and less downtime. A stainless steel cover strip is friction-free on the outside and does not allow any particles to form there. This makes the drives in ...
© Festo SE & Co. KG
2024/09/18
|
ワールドワイド
Precise control of inert gases
Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right ...
プレスリリースを閲覧する
Wherever inert gases need to be precisely controlled, the mass flow controller VEFC from Festo is the right choice. Thanks to piezo technology, it is compact and flexible, and offers an excellent price/performance ratio. It is especially suitable for use in electronics manufacturing, food production, and anywhere in machine building where shielding gas is required.
© Festo SE & Co. KG
VEFC mass flow controller
Compact and flexible thanks to piezo technology: the mass flow controller VEFC.
© Festo SE & Co. KG
2024/09/04
|
アイルランド, イギリス
Festo Controlled Pneumatics
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new ...
プレスリリースを閲覧する
Controlled Pneumatics is the rapidly evolving compressed air technology from Festo that is opening new applications for pneumatics. The technology delivers more precision and control than ever, while having the potential to dramatically reduce energy use. This is clearly demonstrated in the VTEP: the first proportional valve terminal on the market, offering high precision, fast response times, and dynamic control.
Japanese translation unavailable for Jetzt noch mehr hochwertige elektrische Automatisierungstechnik.
© Festo SE & Co. KG
2024/04/24
|
ワールドワイド
Pneumatics Makes a Technological Leap with Piezo
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new ...
プレスリリースを閲覧する
Controlled Pneumatics is the revolutionary compressed air technology from Festo that is opening up new perspectives for pneumatics. Thanks to this technology, the pressure control of the compact proportional valve terminal VTEP is extremely sensitive, down to less than 1 mbar. This is perfect for applications such as wafer polishing or patch clamping in life science. In addition, Controlled Pneumatics uses high-precision piezo valves to reduce ...
© Festo SE & Co. KG
VTEP - use in battery production
The VTEP is suitable for the web control of battery foils, for example.
© Festo SE & Co. KG
VTEP - use in photolithography
Valves such as the VTEP are also used as pilot valves for media valves. In photolithography, for example, a light-resistant layer has to be precisely applied to wafers. A suck-back function ensures that no excess paint escapes.
© Festo SE & Co. KG
Polishing of wafers with VTEP
High-precision control of 5 pressure zones for extremely gentle polishing of wafers with VTEP
© Festo SE & Co. KG
Proportional valve terminal VTEP
Very compact: 10 working channels on an overall width of less than 120 mm