© Festo SE & Co. KG
High pressure lab
High-pressure laboratory at Festo: here, components of high-pressure pneumatics up to 40 bar are developed for the production of PET bottles in the stretch blow moulding process for linear and rotary machines.
Japanese translation unavailable for PMMI & Festo Didactic Join Forces on Workforce Development .
© Festo SE & Co. KG
VTUG
Reliable: The cylinders are controlled by the VTUG valve terminal.
© Festo SE & Co. KG
2022/05/27
|
ワールドワイド
Save 30 per cent volume
Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the ...
プレスリリースを閲覧する
Portugal is the cork world champion: with the largest acreage under cork oaks, the Portuguese are also the largest cork exporters worldwide. Although cork itself is light, it is all the more voluminous if it is packaged inefficiently. In order to save energy and CO₂ emissions during transport, the ESI Group developed a system for packaging corks that requires 30 per cent less packaging volume and does without plastic. On board: automation ...
© Festo SE & Co. KG
DSNU
Robust: the 20 DSNU round cylinders from Festo's core range press the corks together while they are sucked in by the vacuum cups.
© Festo SE & Co. KG
Cork packaging_2
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.
© Festo SE & Co. KG
Cork packaging_1
The robot arm sucks in the corks with vacuum suction cups on its gripper and places them in the cartons to save space.
© Festo SE & Co. KG
2022/04/25
|
ワールドワイド
How many users of compressed air know where the weak points in their systems ...
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the ...
プレスリリースを閲覧する
Operating costs for pneumatic equipment can be reduced by up to 60% if system operators put into practice the results and analyses of the Compressed Air Energy Efficiency Audit GFAA by Festo. Energy efficiency experts from Festo use an integrated approach to analyse the entire compressed air system, from the compressor to the application, and recommend measures to reduce energy consumption. Climate protection is also included in the service, since the ...
© Festo SE & Co. KG
Compressed Air Energy Efficiency Audit GFAA
Five-part audit by Festo: the Compressed Air Energy Efficiency Audit GFAA by Festo can reveal savings of up to 60%.