© Festo SE & Co. KG
PROFINET bus interfaces from Festo
The new PROFINET bus interfaces from Festo: new features for more applications, including in the process industry.
© Festo SE & Co. KG
Valve terminal CPX-MPA with bus module
Valve terminal CPX-MPA with the new bus module CPX-FB43: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
Valve terminal CPX-VTSA with bus module
Valve terminal CPX-VTSA with the new bus module CPX-FB44/45: Festo has upgraded its PROFINET bus interfaces for the CPX automation platform.
© Festo SE & Co. KG
2021/05/25
|
ワールドワイド
Great strides into the digital future
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for ...
プレスリリースを閲覧する
Digitalisation and artificial intelligence (AI) are mega trends that are also opening up the potential for savings in all phases of a plant's lifecycle in process automation. A digital field device, the Festo Motion Terminal VTEM, is already available. Festo Dashboards also visualise plant conditions and even artificial intelligence is no longer far removed from becoming a reality in process automation.